DOCA0271EN-00

Motor One Direction - SIL Stop, W. Cat 1/2

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 1 and Category 2 according to ISO 13849.

The AvMotorOneDirectionSILStop function block is used to manage a motor in one direction with Stop Category 0 or Stop Category 1* function compliance for Wiring Category 1 and Category 2.

AvMotorOneDirectionSILStop Function Block

AvMotorOneDirectionSILStop Input Interface

Input

Data Type

Description

RecordToUChannel1

BOOL

If this input is set to TRUE, the corresponding Time of Use Channel increments, based on measured energy for the selected avatar. This ToU recording continues for the enabled channels until they are disabled.

RecordToUChannel2

BOOL

RecordToUChannel3

BOOL

RecordToUChannel4

BOOL

ResetMaxIRMS

BOOL

If this input is set to TRUE, the maximum average Irms current value and the timestamp are reset.

ResetTrip

BOOL

If this input is set to TRUE, detected trips whose trip reset conditions have been met will reset for this avatar.

ResetTripCntrs

BOOL

If this input is set to TRUE, all trip counters are reset for this avatar.

ResetAlarmCntrs

BOOL

If this input is set to TRUE, all alarm counters are reset for this avatar.

RunFwdCmd

BOOL

If this input is set to TRUE, the avatar forward switch is closed.

AvMotorOneDirectionSILStop Output Interface

Output

Data Type

Description

AssetAlarm

BOOL

If this output is set to TRUE, a power device within the avatar has reached or exceeded 90% of the expected durability (per avatar parameter).

AvgIRMS

DINT

Indicates the average of the most recent phase current Irms values. (Unit: mA)

AvgIRMS_O

DINT

Indicates the average of the most recent phase current Irms overflow values. (Unit: mA)

LoadRunning

BOOL

If this output is set to TRUE, a Run or Close command has been executed, and current is flowing in the poles (equivalent to motor running but also for non-motor avatars).

LoadStarting

BOOL

If this output is set to TRUE, the motor is in start phase.

Ready

BOOL

Indicates TRUE if the function block is ready to receive an execute command.

ReadyToReset

BOOL

If this output is set to TRUE, the avatar meets the trip reset conditions and can be reset with a trip reset command.

RunFwdStatus

BOOL

If this output is set to TRUE, the avatar forward switch is closed.

Tripped

BOOL

If this output is set to TRUE, a protection trip event has been detected by the avatar.

UpstreamVltg1

BOOL

If this output is set to TRUE, the avatar has detected that upstream main power is present for the first starter/power device in this avatar (breaker closed).

Alarm

BOOL

If this output is set to TRUE, a protection alarm has been detected by the avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.