DOCA0271EN-00

Avatar Acyclic Function Blocks

The Avatar_Control function block returns the status of the acyclic data for the individual avatar. In the example below, the AvMotorOneDirection_Control function block is displayed. The same set of acyclic data is available for all avatars, not including the System avatar, analog I/O, and the digital I/O.

AvMotorOneDirection_Control Function Block

Avatar Control Output Interface

Output

Data Type

Description

CurrentPhaseUnbalanceTrip

BOOL

The avatar has detected the conditions to cause a current phase unbalance trip event.

CurrentPhaseUnbalanceAlarm

BOOL

The avatar has detected the conditions to cause a current phase unbalance event.

CurrrentPhaseLossTrip

BOOL

The avatar has detected the conditions to cause a current phase loss trip event.

CurrrentPhaseReversalTrip

BOOL

The avatar has detected the conditions to cause a current phase reversal trip event.

GroundCurrentTrip

BOOL

The avatar has detected the conditions to cause a ground current trip event.

GroundCurrentAlarm

BOOL

The avatar has detected the conditions to cause a ground current event.

JamTrip

BOOL

The avatar has detected the conditions to cause a jam trip event.

JamAlarm

BOOL

The avatar has detected the conditions to cause a jam event.

LongStartTrip

BOOL

The avatar has detected the conditions to cause a long start trip event.

MotorOverheatTrip

BOOL

The motor temperature has increased above the motor overheat trip level.

MotorOverheatAlarm

BOOL

The motor temperature has increased above the motor overheat level.

MotorTemperature

INT

Indicates the temperature of the motor in 0.1 °C scaling unit. Depending on temperature sensor type, the range is:

  • −200 to +850°C (−328 to +1562°F) (for PT100)

  • −200 to +600°C (−328 to +1112°F) (for PT1000)

  • −60 to +180°C (−76 to +356°F) (for NI 100/1000)

NoTrip

BOOL

No trip has been detected.

NoAlarm

BOOL

No advisory condition has been detected.

OverCurrentTrip

BOOL

The avatar has detected the conditions to cause an overcurrent trip event.

OverCurrentAlarm

BOOL

The avatar has detected the conditions to cause an overcurrent event.

PhaseConfigurationTrip

BOOL

The avatar has detected the conditions to cause a phase configuration trip event.

SILGroup

SINT

Indicates the number of the SIL* group.

StallTrip

BOOL

The avatar has detected the conditions to cause a stall trip event.

ThermalCapacity

INT

Provides the percentage (%) of the thermal capacity of the motor which has been used.

ThermalOverloadTrip

BOOL

The avatar thermal capacity has increased above 100%.

ThermalOverloadAlarm

BOOL

The avatar thermal capacity has increased above the thermal overload level.

TimeToReset

DINT

Estimated time to wait before being able to reset a thermal overload trip. (Unit: s)

TimeToTrip

DINT

Estimated time before a thermal overload trip will occur given the current conditions. (Unit: s)

UnderCurrentTrip

BOOL

The avatar has detected the conditions to cause an undercurrent trip event.

UnderCurrentAlarm

BOOL

The avatar has detected the conditions to cause an undercurrent event.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.