DOCA0271EN-00

Import the Subroutine

Import the subroutine L5X file containing the acyclic data, if present. This file uses the following naming convention: {DeviceName}_Acyclic.L5X.

After import:

  • the subroutines are visible in the Tasks tree

  • the acyclic data buffer is visible in the Controller Tags section

For more information on accessing the device data, see Data Access Example.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.