DOCA0271EN-00

Switch

The AvSwitch function block establishes or interrupts a power line in an electric circuit.

AvSwitch Function Block

AvSwitch Input Interface

Input

Data Type

Description

RunFwdCmd

BOOL

If this input is set to TRUE, the avatar forward switch is closed.

ResetTrip

BOOL

If this input is set to TRUE, detected trips whose trip reset conditions have been met will reset for this avatar.

ResetAlarmCntrs

BOOL

If this input is set to TRUE, all alarm counters are reset for this avatar.

ResetTripCntrs

BOOL

If this input is set to TRUE, all trip counters are reset for this avatar.

ResetMaxIRMS

BOOL

If this input is set to TRUE, the maximum average Irms current value and the timestamp are reset.

AvSwitch Output Interface

Output

Data Type

Description

Ready

BOOL

Indicates TRUE if the function block is ready to receive an execute command.

RunFwdStatus

BOOL

If this output is set to TRUE, the avatar forward switch is closed.

Tripped

BOOL

If this output is set to TRUE, a protection trip event has been detected by the avatar.

Alarm

BOOL

If this output is set to TRUE, a protection alarm has been detected by the avatar.

UpstreamVltg1

BOOL

If this output is set to TRUE, the avatar has detected that upstream main power is present for the first starter/power device in this avatar (breaker closed).

AssetAlarm

BOOL

If this output is set to TRUE, a power device or SIL* starter within the avatar has reached or exceeded 90% of the expected durability (per avatar parameter).

LoadRunning

BOOL

If this output is set to TRUE, a Run or Close command has been executed, and current is flowing in the poles (equivalent to motor running but also for non-motor avatars).

ReadyToReset

BOOL

If this output is set to TRUE, the avatar meets the trip reset conditions and can be reset with a trip reset command.

AvgIRMS

DINT

Indicates the average of the most recent phase current Irms values. (Unit: mA)

AvgIRMS_O

DINT

Indicates the average of the most recent phase current Irms overflow values.(Unit: mA)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.