DOCA0271EN-00

General Information

TeSys island add-on instructions provide function blocks to support developing applications and to control avatar modules. Avatar modules are digital function objects managed by the TeSys island system. The system interacts with power devices and accessories such as the analog I/O devices. The avatar modules are configured on the TeSys island , and the bus coupler (via the System avatar) manages fieldbus communication with the controller.

The configuration of the TeSys island modules is managed by the TeSys island Device Type Manager (DTM). For further information, refer to the TeSys island DTM Library Online Help.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.