DOCA0271EN-00

System Energy Management

The AvSystem1_Energy function block returns the status of the acyclic energy data of the System avatar.

AvSystem1_Energy Function Block

AvSystem1_Energy Output Interface

Output

Data Type

Description

ActiveEnergyChannel1

DINT

Channel 1: ToU (Time of Use) total active energy value.

ActiveEnergyChannel1_O

BOOL

Channel 1: ToU (Time of Use) total active energy overflow value.

ActiveEnergyChannel2

DINT

Channel 2 :ToU (Time of Use) total active energy value.

ActiveEnergyChannel2_O

BOOL

Channel 2: ToU (Time of Use) total active energy overflow value.

ActiveEnergyChannel3

DINT

Channel 3: ToU (Time of Use) total active energy value.

ActiveEnergyChannel3_O

BOOL

Channel 3: ToU (Time of Use) total active energy overflow value.

ActiveEnergyChannel4

DINT

Channel 4: ToU (Time of Use) total active energy value.

ActiveEnergyChannel4_O

BOOL

Channel 4: ToU (Time of Use) total active energy overflow value.

AvgVRMS

INT

Average Vrms voltage on three phases (Unit: V)

Frequency

INT

Main power voltage frequency (line frequency as measured on phase 1). (Unit: Hz)

InstActivePower

DINT

Total active power for the system. (Unit: W)

InstReactivePower

DINT

Total reactive power for the system. (Unit: VAR)

MaxActivePower

DINT

Maximum value of the active power for the system. (Unit: W)

MaxActivePowerTimestamp_cs

SINT

Date and time when the maximum active power value was recorded.

MaxActivePowerTimestamp_D

SINT

MaxActivePowerTimestamp_h

SINT

MaxActivePowerTimestamp_M

SINT

MaxActivePowerTimestamp_min

SINT

MaxActivePowerTimestamp_sec

SINT

MaxActivePowerTimestamp_Y

DINT

MaxAvgVRMS

DINT

Maximum voltage the system measured. (Unit: V)

MaxAvgVRMSTimestamp_cs

SINT

Date and time when maximum average voltage value was recorded.

MaxAvgVRMSTimestamp_D

SINT

MaxAvgVRMSTimestamp_h

SINT

MaxAvgVRMSTimestamp_M

SINT

MaxAvgVRMSTimestamp_min

SINT

MaxAvgVRMSTimestamp_sec

SINT

MaxAvgVRMSTimestamp_Y

DINT

MaxPowerFactor

SINT

True maximum power factor value.

MaxPowerFactorTimestamp_cs

SINT

Date and time when the maximum power factor value was recorded.

MaxPowerFactorTimestamp_D

SINT

MaxPowerFactorTimestamp_h

SINT

MaxPowerFactorTimestamp_M

SINT

MaxPowerFactorTimestamp_min

SINT

MaxPowerFactorTimestamp_sec

SINT

MaxPowerFactorTimestamp_Y

DINT

MaxReactivePower

DINT

Maximum value of the reactive power for the system. (Unit: VAR)

MaxReactivePowerTimestamp_cs

SINT

Date and time when the maximum reactive power value was recorded.

MaxReactivePowerTimestamp_D

SINT

MaxReactivePowerTimestamp_h

SINT

MaxReactivePowerTimestamp_M

SINT

MaxReactivePowerTimestamp_min

SINT

MaxReactivePowerTimestamp_sec

SINT

MaxReactivePowerTimestamp_Y

DINT

MaxUnbalancedVltg

SINT

Maximum unbalance voltage in percent (%).

MaxUnbalancedVltgTimestamp_cs

SINT

Date and time of maximum unbalance voltage.

MaxUnbalancedVltgTimestamp_D

SINT

MaxUnbalancedVltgTimestamp_h

SINT

MaxUnbalancedVltgTimestamp_M

SINT

MaxUnbalancedVltgTimestamp_min

SINT

MaxUnbalancedVltgTimestamp_sec

SINT

MaxUnbalancedVltgTimestamp_Y

DINT

MinPowerFactor

SINT

True minimum power factor value.

MinPowerFactorTimestamp_cs

SINT

Date and time when the minimum power factor value was recorded.

MinPowerFactorTimestamp_D

SINT

MinPowerFactorTimestamp_h

SINT

MinPowerFactorTimestamp_M

SINT

MinPowerFactorTimestamp_min

SINT

MinPowerFactorTimestamp_sec

SINT

MinPowerFactorTimestamp_Y

DINT

PowerFactor

SINT

True power factor value.

TotalActiveEnergy

DINT

Total active energy value for all avatars in the system with Energy Monitoring Enabled. (Unit: Watt-hours)

TotalActiveEnergy_O

BOOL

Total active energy overflow value for all avatars in the system with Energy Monitoring Enabled.

TotalReactiveEnergy

DINT

Total reactive energy value for all avatars in the system with Energy Monitoring Enabled. (Unit: VAR-hours)

TotalReactiveEnergy_O

BOOL

Total reactive energy overflow value for all avatars in the system with Energy Monitoring Enabled.

UnbalancedVltg

SINT

Unbalance voltage in percent (%).

VltgDipCntr

DINT

Voltage dip counter

VltgPhaseOrderACB

BOOL

If this output is set to TRUE, the phase order is ACB (FALSE = phase order ABC).

VltgSwellCntr

DINT

Voltage swell counter

VoltageDipMagnitude1

DINT

Maximum voltage magnitude for a voltage dip. (Unit: V)

VoltageDipMagnitude5

DINT

Maximum voltage magnitude for a voltage dip. (Unit: V)

VoltageDipStartDate1_cs

SINT

Start time stamp of the voltage dip.

VoltageDipStartDate1_D

SINT

VoltageDipStartDate1_h

SINT

VoltageDipStartDate1_M

SINT

VoltageDipStartDate1_min

SINT

VoltageDipStartDate1_sec

SINT

VoltageDipStartDate1_Y

DINT

VoltageDipStartDate5_cs

SINT

Start time stamp of the voltage dip.

VoltageDipStartDate5_D

SINT

VoltageDipStartDate5_h

SINT

VoltageDipStartDate5_M

SINT

VoltageDipStartDate5_min

SINT

VoltageDipStartDate5_sec

SINT

VoltageDipStartDate5_Y

DINT

VoltageDipStopDate1_cs

SINT

Stop time stamp of the voltage dip.

VoltageDipStopDate1_D

SINT

VoltageDipStopDate1_h

SINT

VoltageDipStopDate1_M

SINT

VoltageDipStopDate1_min

SINT

VoltageDipStopDate1_sec

SINT

VoltageDipStopDate1_Y

DINT

VoltageDipStopDate5_cs

SINT

Stop time stamp of the voltage dip.

VoltageDipStopDate5_D

SINT

VoltageDipStopDate5_h

SINT

VoltageDipStopDate5_M

SINT

VoltageDipStopDate5_min

SINT

VoltageDipStopDate5_sec

SINT

VoltageDipStopDate5_Y

DINT

VoltageSwellMagnitude1

DINT

Maximum voltage magnitude for a voltage swell. (Unit: V)

VoltageSwellMagnitude5

DINT

VoltageSwellStartDate1_cs

SINT

Start time stamp of the voltage swell.

VoltageSwellStartDate1_D

SINT

VoltageSwellStartDate1_h

SINT

VoltageSwellStartDate1_M

SINT

VoltageSwellStartDate1_min

SINT

VoltageSwellStartDate1_sec

SINT

VoltageSwellStartDate1_Y

DINT

VoltageSwellStartDate5_cs

SINT

VoltageSwellStartDate5_D

SINT

VoltageSwellStartDate5_h

SINT

VoltageSwellStartDate5_M

SINT

VoltageSwellStartDate5_min

SINT

VoltageSwellStartDate5_sec

SINT

VoltageSwellStartDate5_Y

DINT

VoltageSwellStopDate1_cs

SINT

Stop time stamp of the voltage swell.

VoltageSwellStopDate1_D

SINT

VoltageSwellStopDate1_h

SINT

VoltageSwellStopDate1_M

SINT

VoltageSwellStopDate1_min

SINT

VoltageSwellStopDate1_sec

SINT

VoltageSwellStopDate1_Y

DINT

VoltageSwellStopDate5_cs

SINT

VoltageSwellStopDate5_D

SINT

VoltageSwellStopDate5_h

SINT

VoltageSwellStopDate5_M

SINT

VoltageSwellStopDate5_min

SINT

VoltageSwellStopDate5_sec

SINT

VoltageSwellStopDate5_Y

DINT

VRMSPhase1

DINT

Average Vrms voltage between L1 and neutral. (Unit: V)

VRMSPhase2

DINT

Average Vrms voltage between L2 and neutral. (Unit: V)

VRMSPhase3

DINT

Average Vrms voltage between L3 and neutral. (Unit: V)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.