Switch - SIL Stop, W. Cat 3/4
The AvSwitchSILStopCat34function block establishes or interrupts a power line in an electric circuit with Stop Category 0 or Stop Category 1* function compliance for Wiring Category 3 and Category 4.
AvSwitchSILStopCat34 Input Interface
| Input | Data Type | Description |
| Run1Cmd | BOOL |
If this input is set to TRUE, the avatar forward primary switch is closed. |
| Run2Cmd | BOOL |
If this input is set to TRUE, the avatar forward redundant switch is closed. |
| ResetTrip | BOOL |
If this input is set to TRUE, detected trips whose trip reset conditions have been met will reset for this avatar. |
| ResetAlarmCntrs | BOOL |
If this input is set to TRUE, all alarm counters are reset for this avatar. |
| ResetTripCntrs | BOOL |
If this input is set to TRUE, all trip counters are reset for this avatar. |
| ResetMaxIRMS | BOOL |
If this input is set to TRUE, the maximum average Irms current value and the timestamp are reset. |
AvSwitchSILStopCat34 Output Interface
| Output | Data Type | Description |
| Ready | BOOL |
Indicates TRUE if the function block is ready to receive an execute command. |
| Run1Status | BOOL |
If this output is set to TRUE, the avatar forward primary switch is closed. |
| Run2Status | BOOL |
If this output is set to TRUE, the avatar forward redundant switch is closed. |
| Tripped | BOOL |
If this output is set to TRUE, a protection trip event has been detected by the avatar. |
| Alarm | BOOL |
If this output is set to TRUE, a protection alarm has been detected by the avatar. |
| UpstreamVltg1 | BOOL |
If this output is set to TRUE, the avatar has detected that upstream main power is present for the first starter/power device in this avatar (breaker closed). |
| UpstreamVltg2 | BOOL |
If this output is set to TRUE, the avatar has detected that upstream main power is present for the second starter/power device in this avatar (breaker closed). |
| AssetAlarm | BOOL |
If this output is set to TRUE, a power device or SIL* starter within the avatar has reached or exceeded 90% of the expected durability (per avatar parameter). |
| LoadRunning | BOOL |
If this output is set to TRUE, a Run or Close command has been executed, and current is flowing in the poles (equivalent to motor running but also for non-motor avatars). |
| ReadyToReset | BOOL |
If this output is set to TRUE, the avatar meets the trip reset conditions and can be reset with a trip reset command. |
| AvgIRMS | DINT |
Indicates the average of the most recent phase current Irms values. (Unit: mA) |
| AvgIRMS_O | DINT |
Indicates the average of the most recent phase current Irms overflow values. (Unit: mA) |