DOCA0271EN-00

System Diagnostic

The AvSystem1_Diagnostic function block returns the status of the acyclic diagnostic data of the System avatar.

AvSystem1_Diagnostic Function Block

AvSystem1_Diagnostic Output Interface

Output

Data Type

Description

ComErrorCntr

DINT

Number of detected errors for the fieldbus communication.

AlarmsCntr

DINT

Number of detected alarms for the system.

MinorEvtCntr

DINT

Number of detected minor events for the system.

MinorEvtRegister1_Y

DINT

Information on a detected minor event. MinorEvtRegister1_ = most recent.

MinorEvtRegister1_M

SINT

MinorEvtRegister1_D

SINT

MinorEvtRegister1_h

SINT

MinorEvtRegister1_min

SINT

MinorEvtRegister1_sec

SINT

MinorEvtRegister1_cs

SINT

MinorEvtRegister1_EventIdentifier

DINT

. . .

. . .

. . .

MinorEvtRegister5_Y

DINT

Information on a detected minor event.

MinorEvtRegister5_M

SINT

MinorEvtRegister5_D

SINT

MinorEvtRegister5_h

SINT

MinorEvtRegister5_min

SINT

MinorEvtRegister5_sec

SINT

MinorEvtRegister5_cs

SINT

MinorEvtRegister5_EventIdentifier

DINT

SILStarterStopMsgGrp1SILGroupNotPresent

BOOL

Status for SIL* Groups 1– 10:

  • NotPresent = SIL Group not present in system configuration

  • AvatarDeviceEvent = SIL Group impacted by avatar device event

  • SILStartersNotOpen = SIL Group Stop command received; SIL starters not open yet

  • AllStartersNotOpen = SIL Group Stop command successfully issued; all SIL starters are open

  • CmdIssuedOneTerminal = SIL Group Stop command issued to only one SIM input channel (jumper or SIM input wiring is causing an issue), but SIL starters did successfully open

  • NormalOperation = Normal operation; SIL starters can be open or closed

SILStarterStopMsgGrp1AvatarDeviceEvent

BOOL

SILStarterStopMsgGrp1SILStartersNotOpen

BOOL

SILStarterStopMsgGrp1AllSILStartersOpen

BOOL

SILStarterStopMsgGrp1CmdOnlyOneTerminal

BOOL

SILStarterStopMsgGrp1NormalOperation

BOOL

. . .

. . .

SILStarterStopMsgGrp10SILGroupNotPresent

BOOL

SILStarterStopMsgGrp10AvatarDeviceEvent

BOOL

SILStarterStopMsgGrp10SILStartersNotOpen

BOOL

SILStarterStopMsgGrp10AllSILStartersOpen

BOOL

SILStarterStopMsgGrp10CmdOnlyOneTerminal

BOOL

SILStarterStopMsgGrp10NormalOperation

BOOL

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.