DOCA0271EN-00

System Asset Management

The AvSystem1_AssetManagement function block returns the status of the acyclic asset management data of the System avatar.

AvSystem1_AssetManagement Function Block

AvSystem1_AssetManagement Output Interface

Output

Data Type

Description

MacAddress_XX

INT

MAC address of the device XX.

MacAddress_YY

INT

MAC address of the device YY.

MacAddress_ZZ

INT

MAC address of the device ZZ.

MacAddress_UU

INT

MAC address of the device UU.

MacAddress_VV

INT

MAC address of the device VV.

MacAddress_WW

INT

MAC address of the device WW.

TimeModuleOn

DINT

This register indicates the time that the module has been powered on in its lifetime (Unit: h).

TimeModuleOn_O

BOOL

This register indicates the overflow time that the module has been powered on in its lifetime.

EventCntr

DINT

This register indicates number of times this module has experienced a detected device error (Unit: h). This value does not include detected device events which corrupt or prevent the saving of the non-volatile memory.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.