DOCA0271EN-00

Create Instances of the AOIs

When creating an instance of an AOI, you must reference the module and the acyclic data buffer. Depending on the data present in the AOI (cyclic or acyclic), there are one or two tags to reference.

  1. Enter the Main Routine by double-clicking it within the Tasks tree.

  2. Add an AOI from the add-on list.

  3. Fill in the reference tags for each In/Out parameter. These tags are in the Controller Tags list with names matching the In/Out Parameters.

  4. Create an instance of the AOI and name it.

The AOI is now fully configured and ready for use.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.