DOCA0271EN-00

Power Interface with I/O (Control)

The AvPowerInterfacewit function block is used to monitor current and control an external power device, such as a solid-state relay, soft starter, or variable speed drive.

AvPowerInterfacewit Function Block

AvPowerInterfacewit Input Interface

Input

Data Type

Description

LQ1Cmd

BOOL

If this input is set to TRUE, the logical output 1 is set to TRUE.

LQ2Cmd

BOOL

If this input is set to TRUE, the logical output 2 is set to TRUE.

ResetTrip

BOOL

If this input is set to TRUE, detected trips whose trip reset conditions have been met will reset for this avatar.

ResetAlarmCntrs

BOOL

If this input is set to TRUE, all alarm counters are reset for this avatar.

ResetTripCntrs

BOOL

If this input is set to TRUE, all trip counters are reset for this avatar.

ResetMaxIRMS

BOOL

If this input is set to TRUE, the maximum average Irms current value and the timestamp are reset.

RecordToUChannel1

BOOL

If this input is set to TRUE, the corresponding Time of Use Channel increments, based on measured energy for the selected avatar. This ToU recording continues for the enabled channels until they are disabled.

RecordToUChannel2

BOOL

RecordToUChannel3

BOOL

RecordToUChannel4

BOOL

AvPowerInterfacewit Output Interface

Output

Data Type

Description

Ready

BOOL

Indicates TRUE if the function block is ready to receive an execute command.

LQ1Status

BOOL

If this output is set to TRUE, the logical output 1 is set to TRUE.

Tripped

BOOL

If this output is set to TRUE, a protection trip event has been detected by the avatar.

Alarm

BOOL

If this output is set to TRUE, a protection alarm has been detected by the avatar.

UpstreamVltg1

BOOL

If this output is set to TRUE, the avatar has detected that upstream main power is present for the first starter/power device in this avatar (breaker closed).

LQ2Status

BOOL

If this output is set to TRUE, the logical output 2 is set to TRUE.

LoadRunning

BOOL

If this output is set to TRUE, a Run or Close command has been executed, and current is flowing in the poles (equivalent to motor running but also for non-motor avatars).

ReadyToReset

BOOL

If this output is set to TRUE, the avatar meets the trip reset conditions and can be reset with a trip reset command.

LI1

BOOL

If this output is set to TRUE, the logical input 1 of the avatar is set to TRUE.

LI2

BOOL

If this output is set to TRUE, the logical input 2 of the avatar is set to TRUE.

LoadStarting

BOOL

If this output is set to TRUE, the motor is in start phase.

AvgIRMS

DINT

Indicates the average of the most recent phase current Irms values. (Unit: mA)

AvgIRMS_O

DINT

Indicates the average of the most recent phase current Irms overflow values.(Unit: mA)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.