DOCA0271EN-00

Function Blocks

TeSys™ island function blocks integrated with Studio 5000® are fieldbus independent and have no logic instructions. The inputs and outputs of the function blocks are linked to the process image (cyclic data) without any modifications. Inputs and outputs, which are not part of the process image, are exchanged via acyclic communication methods.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.