DOCA0271EN-00

Import the Add-on Instructions

Import the add-on instructions (AOIs) as shown below. This file uses the following naming conventions: {DeviceName}_Aoi.L5X

After import, the AOIs are visible in the project tree.

Each AOI contains either cyclic or acyclic data, which is indicated by the following naming convention:

  • Cyclic data contains only the name of the avatar.

  • Acyclic data contains the name of the avatar followed by an underscore (_) and the name of the acyclic data object.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.