DOCA0271EN-00

Calling Acyclic Data

When calling acyclic data, you must add a Jump To Subroutine operation to the Main Routine. The subroutine needed for the target AOI matches the associated avatar.

This action pushes or pulls data, depending on the type of data the explicit message is accessing.

  1. Open the subroutine.

  2. Toggle the Examine If Open bit on the rung containing the message associated with the target AOI.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.