DOCA0271EN-00

Pump

The AvPump function block is used to manage a pump.

AvPump Function Block

AvPump Input Interface

Input Data Type Description
RunFwdCmd BOOL

If this input is set to TRUE, the avatar forward switch is closed.

ResetTrip BOOL

If this input is set to TRUE, detected trips whose trip reset conditions have been met will reset for this avatar.

ResetAlarmCntrs BOOL

If this input is set to TRUE, all alarm counters are reset for this avatar.

ResetTripCntrs BOOL

If this input is set to TRUE, all trip counters are reset for this avatar.

ResetMaxIRMS BOOL

If this input is set to TRUE, the maximum average Irms current value and the timestamp are reset.

RecordToUChannel1 BOOL

If this input is set to TRUE, the corresponding Time of Use Channel increments, based on measured energy for the selected avatar. This ToU recording continues for the enabled channels until they are disabled.

RecordToUChannel2 BOOL
RecordToUChannel3 BOOL
RecordToUChannel4 BOOL

AvPump Output Interface

Output Data Type Description
Ready BOOL

Indicates TRUE if the function block is ready to receive an execute command.

RunFwdStatus BOOL

If this output is set to TRUE, the avatar forward switch is closed.

Tripped BOOL

If this output is set to TRUE, a protection trip event has been detected by the avatar.

Alarm BOOL

If this output is set to TRUE, a protection alarm has been detected by the avatar.

UpstreamVltg1 BOOL

If this output is set to TRUE, the avatar has detected that upstream main power is present for the first starter/power device in this avatar (breaker closed).

AssetAlarm BOOL

If this output is set to TRUE, a power device or SIL* starter within the avatar has reached or exceeded 90% of the expected durability (per avatar parameter).

LoadRunning BOOL

If this output is set to TRUE, a Run or Close command has been executed, and current is flowing in the poles (equivalent to motor running but also for non-motor avatars).

ReadyToReset BOOL

If this output is set to TRUE, the avatar meets the trip reset conditions and can be reset with a trip reset command.

LocalfwdCmdSts BOOL

If this output is set to TRUE, the avatar logic is controlled by commands received on digital inputs, and PLC commands are ignored.

BypassCmdSts BOOL

If this output is set to TRUE, the avatar will continue operation and not stop due to a trip.

ManualModeOverrideStatus BOOL

If this output is set to TRUE, the avatar is controlled by local command and PV control when in manual mode.

LoadStarting BOOL

If this output is set to TRUE, the motor is in start phase.

AvgIRMS DINT

Indicates the average of the most recent phase current Irms values. (Unit: mA)

AvgIRMS_O DINT

Indicates the average of the most recent phase current Irms overflow values. (Unit: mA)

PVInput0 INT

Returns the measured value of the PV Input.

PVInput1 INT
PVInput2 INT
PVInput3 INT
PvInput4 INT
PVSwitch0 BOOL

Positive Logic - A PV Switch input ON or a PV Input above the PV Control Level represents an ON command.

Negative Logic - A PV Switch input OFF or a PV Input below the PV Control Level represents an ON command.

PVSwitch1 BOOL
PVSwitch2 BOOL
PVSwitch3 BOOL
PVSwitch4 BOOL
PVControlInputStatus0 BOOL

If this output is set to TRUE, a command has been sent to the avatar from a PV Control Input.

PVControlInputStatus1 BOOL

If this output is set to TRUE, a command has been sent to the avatar from a PV Control Input.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.