DOCA0271EN-00

System

The AvSystem function block returns the status and resets the cyclic diagnostic and energy data of the System avatar.

AvSystem Function Block

AvSystem Input Interface

Input

Data Type

Description

ResetVltgFlctnStatus

BOOL

If this input is set to TRUE, the value of the parameter ResetVltgFlctnStatus is reset.

ResetMaxUnbalanceVltg

BOOL

If this input is set to TRUE, the value of the parameter ResetMaxUnbalanceVltg is reset.

ResetMaxVRMS

BOOL

If this input is set to TRUE, the value of the parameter ResetMaxVRMS is reset.

ResetComErrorCntr

BOOL

If this input is set to TRUE, the counter of detected errors for the fieldbus communication is set to 0.

ResetMinorEvtCntr

BOOL

If this input is set to TRUE, the counter of detected minor events for the system is set to 0.

ResetAlarmCntr

BOOL

If this input is set to TRUE, the counter of detected alarms for the system is set to 0.

ResetSystem

BOOL

If this input is set to TRUE, the system is reset.

AvSystem Output Interface

Output

Data Type

Description

UpstreamVltgFlctnStatus

BOOL

If this output is set to TRUE, a voltage dip or swell is detected. Can be reset with ResetVltgFlctnStatus.

SILStarterStopStatus

BOOL

Status of SIL* Starter Stop 0 function. If this output is set to FALSE, no SIL group has received a SIL Starter Stop command.

CtrlVltgFlctn

BOOL

If this output is set to TRUE, a control voltage fluctuation is detected.

Preoperational

BOOL

If this output is set to TRUE, the System avatar is in Preoperational mode.

Operational

BOOL

If this output is set to TRUE, the System avatar is in Operational mode. For detailed information on machine states, refer to the TeSys island – System, Installation, and Operation Guide .

TestMode

BOOL

If this output is set to TRUE, the System avatar is in Test mode.

MinorEvt

BOOL

If this output is set to TRUE, the System avatar is in Minor Event mode.

ForceMode

BOOL

If this output is set to TRUE, the System avatar is in Force mode.

DegradedMode

BOOL

If this output is set to TRUE, the System avatar is in Degraded mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.