DOCA0271EN-00

Add an Ethernet Bridge

To add an Ethernet bridge:

  1. Launch the Studio 5000® software.

  2. Click Create > New Project.

    A new project opens.

  3. Select your PLC from the list of available PLCs.

  4. Enter a Name for the PLC. Click Next.

  5. Make any changes necessary for the PLC. Click Finish.

    Your PLC module is added to the I/O Configuration tree.

  6. Add an Ethernet bridge to its backplane.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.