System Combined Output
The CombinedSystemOutput function block returns the energy information of the System avatar, resets the energy registers of the System avatar, and sets the energy preset values of the avatars (A2, A3, etc.).
CombinedSystemOutput Input Interface
|
Input |
Data Type |
Description |
|---|---|---|
|
ResetVltgDipCntr |
BOOL |
If this input is set to TRUE, the value of the parameter ResetVltgDipCntr is reset. |
|
ResetVltgSwellCntr |
BOOL |
If this input is set to TRUE, the value of the parameter ResetVltgSwellCntr is reset. |
|
ResetMaxActivePower |
BOOL |
If this input is set to TRUE, the value of the parameter MaxActivePower and the associated time stamp MaxActivePowerTimestamp are reset. |
|
ResetMaxReactivePower |
BOOL |
If this input is set to TRUE, the value of the parameter MaxReactivePower and the associated time stamp MaxReactivePowerTimestamp are reset. |
|
ResetMinPowerFactor |
BOOL |
If this input is set to TRUE:
|
|
ResetMaxPowerFactor |
BOOL |
If this input is set to TRUE:
|
|
ResetReactiveEnergy |
BOOL |
If this input is set to TRUE, the value of the parameter ReactiveEnergy is reset. |
|
ResetActiveEnergy |
BOOL |
If this input is set to TRUE, the value of the parameter ActiveEnergy is reset. |
|
A2_SetActiveEnergy |
BOOL |
Command to set the TotalActiveEnergy value to TotalActiveEnergyPreset value. |
|
A2_SetReactiveEnergy |
BOOL |
Command to set the TotalReactiveEnergy value to TotalReactiveEnergyPreset value. |
|
A2_SetValueActiveEnergy |
DINT |
Value to preset the TotalActiveEnergy, will take effect on a TRUE command to SetActiveEnergy (Unit: Watt-hours) |
|
A2_SetValueReactiveEnergy |
DINT |
Value to preset the TotalReactiveEnergy, will take effect on a TRUE command to SetReactiveEnergy (Unit: VAR-hours) |
|
… |
… |
… |
|
A7_SetActiveEnergy |
BOOL |
Command to set the TotalActiveEnergy value to TotalActiveEnergyPreset value. |
|
A7_SetReactiveEnergy |
BOOL |
Command to set the TotalReactiveEnergy value to TotalReactiveEnergyPreset value. |
|
A7_SetValueActiveEnergy |
DINT |
Value to preset the TotalActiveEnergy, will take effect on a TRUE command to SetActiveEnergy (Unit: Watt-hours) |
|
A7_SetValueReactiveEnergy |
DINT |
Value to preset the TotalReactiveEnergy, will take effect on a TRUE command to SetReactiveEnergy (Unit: VAR-hours) |