DOCA0271EN-00

Asset Management

The DeviceX_AssetManagement function block returns the status of the acyclic asset management data of the specified device.

DeviceX_AssetManagement Function Block

DeviceX_AssetManagement Output Interface

Output

Data Type

Description

TimeDeviceOn

DINT

This register indicates the time that the module has been powered on in its lifetime. (Unit: h)

TimeDeviceOn_O

BOOL

This register indicates the overflow time that the module has been powered on in its lifetime.

TimeSwitchOn

DINT

This register indicates the time the contactor has been in the closed state. (Unit: h)

TimeSwitchOn_O

BOOL

This register indicates the overflow time the contactor has been in the closed state.

EventCntr

DINT

This register indicates number of times this module has experienced a detected device error. This value does not include detected device errors which prevent the saving or corruption of the non-volatile memory.

ContactorCycleCntr

DINT

This register indicates the number of times the contactor has been commanded to the closed state from the open state.

ContactorCycleCntr_O

BOOL

This register indicates the overflow number of times the contactor has been commanded to the closed state from the open state.

DevicePowerCycleCntr

DINT

This register indicates the number of times the device has been powered on.

DevicePowerCycleCntr_O

BOOL

This register indicates the overflow number of times the device has been powered on.

SILStopCntr

DINT

This value indicates the number of mirror relay operations.

SILStopCntr_O

BOOL

This value indicates the overflow number of mirror relay operations.

MaxIRMS

DINT

This register indicates the maximum current the device has measured in its lifetime. (Unit: 100 mA)

AvgIRMS

DINT

Lifetime average current measured by the device (Total Current/Time Current ON). (Unit: mA)

AvgIRMS_O

DINT

Lifetime average current measured by the device (Total Current/Time Current ON) overflow value. (Unit: mA)

MaxAvgVRMS

DINT

This register indicates the maximum voltage the device has measured in its lifetime. (Unit: V)

AvgVRMS

DINT

Average Vrms voltage on three phases. (Unit: V)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.