DOCA0271EN-00

Obtain the L5X Files

Configure the island in the TeSys™ island DTM according to the TeSys island – System, Installation, and Operation Guide. Then, export the L5X files from the TeSys island DTM according to the following procedure.

  1. In the TeSys island DTM, open the TeSys island project you wish to export.

  2. From the drop-down menu, click Device.

  3. Select Export > EDS to L5X File Format.

  4. Click Save.

    The file is saved as a zip file in the following format: island_name.zip.

  5. A notification appears, saying that the L5X files have been created.

    Click OK.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.