0613CT0001

Accessory Dimensional Drawings

IFE Ethernet Interface Dimensions

I/O (Input/Output) Application Module Dimensions

IFM Modbus-SL Interface Dimensions

FDM121 Switchboard Display Dimensions

FDM121 Switchboard Display Mounting Through Panel

FDM121 Switchboard Display Mounting On Panel

FDM128 Switchboard Display Dimensions

FDM128 Switchboard Display Mounting on Panel

 

MasterPacT NT and NW Circuit Breaker Communication

Fixed MasterPacT NT and NW Connection to the Communication Interface Module

Drawout MasterPacT NT and NW Connection to the IO and Communication Interface Module

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.