0613CT0001

Options for Remote Operation

Two options are available for remote operation of MasterPacT circuit breakers: direct connection or a communication network.

NOTE: When remote operation features are used, a minimum of four seconds is required for the spring charging motor (MCH) to completely charge the circuit breaker closing springs prior to actuating the shunt close (XF) device.

The wiring diagrams for these two options are shown below.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.