0613CT0001

IFE Ethernet Interface

IFE Interface

IFE Interface + Gateway

Introduction

The IFE interface and IFE interface + gateway enable low-voltage circuit breakers such as MasterPacT NT/NW or PowerPacT P/R-frame to be connected to an Ethernet network.

IFE Interface

Provides Ethernet access to a single low-voltage circuit breaker.

Function: Interface - one circuit breaker is connected to the IFE interface using its ULP port.

IFE Interface + Gateway

Provides Ethernet access to one or several low-voltage circuit breakers.

Functions:

  • Interface - one circuit breaker is connected to the IFE interface using its ULP port.

  • Gateway: several circuit breakers on a Modbus network are connected using the IFE interface + gateway master Modbus port.

IFE Interface, IFE Interface + Gateway Features

  • Dual 10/100 Mbps Ethernet port for simple daisy chain connection.

  • Device profile web service for discovery of the IFE interface, IFE interface + gateway on the LAN.

  • Ethernet interface for MasterPacTt and PowerPacT circuit breakers.

  • Gateway for Modbus-SL connected devices (IFE interface + gateway only).

  • Embedded set-up web pages.

  • Embedded monitoring web pages.

  • Embedded control web pages.

  • Built-in e-mail alarm notification.

IFE Interface, IFE Interface + Gateway Screen

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.