0613CT0001

Enerlin’X Communication System Components

MasterPacT Circuit Breakers with MicroLogic Trip Units

Ammeter A

  • 3.0 basic protection

  • 5.0 selective protection

  • 6.0 selective + ground-fault protection

Power Meter P

  • 5.0 selective protection

  • 6.0 selective + ground-fault protection

Harmonic Meter H

  • 5.0 selective protection

  • 6.0 selective + ground-fault protection

See MicroLogic 5.0H and 6.0H Trip Units with Harmonic Metering for more information.

Displays

Power Meter

FDM121

One-to-one front display module

SeeFDM121 Display for more information

Operating Assistance Functions

FDM128

One-to-eight front display module

SeeFDM128 Display for more information

Communication

Communication

  • MasterPacT circuit breakers in a communication network

  • I/O application module

  • IFE: Ethernet interface module

  • IFM: Modbus interface module

I/O Module

IFE Module

IFM Module

See FDM121 Display for more information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.