0613CT0001

Ammeter (A) Trip Unit with 24 Vdc Power Supply at F1 and F2

The Ammeter (A) trip unit provides all of the above plus additional functionality when powered by external 24 Vdc power supply:

  • Ammeter and bar graph displays are functional with or without current flowing through the circuit breaker.

  • Trip settings and (Max) current readings can be accessed on the display by pressing navigation button with or without current flowing through the circuit breaker.

  • The ground-fault push-to-trip button works for testing ground fault with or without current flowing through the circuit breaker.

  • Optional Modbus™ communications—also requires a separate 24 Vdc power supply for the circuit breaker communications module.

NOTE: Ground-fault push-to-trip button will also be functional if a service interface, a hand-held test kit, or a full-function test kit is powering the trip unit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.