0613CT0001

Miscellaneous Accessories

Mechanical Operation Counter (CDM)

Mechanical Operation Counter (CDM)

The mechanical operation counter (CDM) registers the total number of operating cycles. One CDM is installed per circuit breaker.

Shutter and Shutter Lock

The shutters automatically block access to the main disconnects when the circuit breaker is in the disconnected, test, or fully withdrawn position.

The shutter lock is used to prevent connection of the circuit breaker or to lock the shutters in the closed position.

Not available on cradles with ArcBlok technology.

UL® Circuit Breaker Shutter

Shutter Lock

Door Escutcheon (CDP)

These door escutcheons provide a frame and seal for the circuit breaker.

Door Escutcheon (NW Fixed)

Door Escutcheon (NW Drawout)

Transparent Cover (CCP) for Door Escutcheon

Transparent Cover (CCP)

The cover is hinged-mounted and locked with a milled head, and is designed to be installed on the door escutcheon.

Drawout MasterPacT NW Remote Racking Device

The remote racking device allows the operator to perform circuit breaker racking operations from a distance of up to 30 feet (9.1 m) away from the circuit breaker using the controller. This distance exceeds the arc flash boundary described in the arc flash safety guidelines outlined in NFPA-70E.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.