0613CT0001

IFE Ethernet Interface Mounting

The IFE interface and IFE interface + gateway are DIN rail mounted devices. A stacking accessory enables the user to connect several IFMs (ULP to Modbus interfaces) to an IFE interface + gateway without additional wiring.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.