0613CT0001

MicroLogic 5.0P & 6.0P Trip Units with Power Metering

Protection Settings

1—Test lamp and indication reset

2—Indication of tripping cause

3—High resolution screen

4—Measurement display

5—Maintenance indicators

6—Protection settings

7—Navigation buttons

8—Overload signal (LED)

9—Long-time rating plug screw

10—Long-time current setting and tripping delay

11—Short-time pickup and

tripping delay

12—Instantaneous pickup

13—Hole for settings lockout pin

14—Electronic push-to-trip

15—Ground-fault pickup and tripping delay

16—Test connector

MicroLogic 6.0P Trip Unit

The adjustable protection functions of the 5.0P and 6.0P trip units are identical to those of MicroLogic A trip unit (overloads, short circuits, equipment ground-fault protection); see MicroLogic 2.0A, 3.0A, 5.0A, & 6.0A Trip Units with Ammeter.

These units also feature:

Fine adjustment: Within the range below the rotary switch setting, fine adjustments of pickups/delays in steps of 1 A/s (except for short-time and ground-fault) are possible on the keypad or remotely by the communication network.

Inverse definite minimum time lag (IDMTL) setting: Coordination with fuse-type or medium-voltage protection systems is optimized by adjusting the long-time delay curve around 6 x Ir axis. This setting provides better coordination with certain loads.

Neutral protection: On three-pole circuit breakers, neutral protection may be set using the keypad or remotely using the communication network to one of four positions:

  • OFF

  • 1/2N (1/2 x In)

  • 1N (1 x In)

  • 2N (2 x In)

NOTE: The neutral protection is disabled if the long-time curve is set to one of the IDMTL protection settings.

Configuring Alarms and Other Protection Functions

When the cover is closed, the keypad may no longer be used to change the protection settings, but it still provides access to the displays for measurements, histories, indicators, etc. Depending on the thresholds and time delays set, the MicroLogic P trip unit monitors current, voltage, power, frequency, and phase sequence. Each threshold overrun may be signalled remotely via the communication network.

Each threshold overrun may be combined with tripping (protection) or an indication carried out by an optional M2C/M6C programmable contact (alarm), or both (protection and alarm).

Maintenance Record

The maintenance record can be consulted using a service interface, a full-function test kit, or remotely via the communication network. It can be used as an aid in troubleshooting and to assist scheduling for device maintenance operations.

Recorded indications include:

  • Highest current measured

  • Operation counter (both cumulative total and total since last reset)

  • Number of test kit connections

  • Number of trips in operating mode

  • Contact wear (MasterPacT NW only)

Load Shedding and Reconnection Parameters

Load shedding and reconnection parameters can be set according to the power or the current flowing through the circuit breaker. Load shedding is carried out by a remote computer via the communication network or by an M2C or M6C programmable contact.

Indication Option via Programmable Contacts

The M2C (two contacts) and M6C (six contacts) programmable contacts may be used to signal threshold overruns or status changes. They can be programmed using the keypad on the MicroLogic P and H trip units or remotely using the communication network. These contacts are required to obtain data from the protective relay functions on Type P and Type H trip units.

MicroLogic 5.0P and 6.0P Trip Unit Settings

Long-Time (RMS) Protection

Current Setting (A)
Tripping Between 1.05 and 1.20 x Ir

Ir = ln x...

IEC:

0.4

0.5

0.6

0.7

0.8

0.9

0.95

0.98

1

Ir = ln x...

UL/ANSI:

0.4

0.45

0.5

0.6

0.63

0.7

0.8

0.9

1

 

Other ranges are available by changing rating plug

Time Delay (s)
Accuracy: 0 to –20%

tr at 1.5 x Ir

12.5

25

50

100

200

300

400

500

600

tr at 6 x Ir

0.5

1

2

4

8

12

16

20

24

tr at 7.2 x Ir

0.34

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

IDMTL Setting

Curve slope

SIT

VIT

EIT

HV Fuse

DT

Thermal Imaging

20 minutes before or after tripping

Short-Time (RMS) Protection

Current Setting (A)
Accuracy: ±10%

lsd = Ir x...

1.5

2

2.5

3

4

5

6

8

10

Time Delay (s)
at 10 x Ir

Settings

I2t OFF

0

0.1

0.2

0.3

0.4

 

I2t ON

0.1

0.2

0.3

0.4

 

tsd

Min. trip time (ms)

20

80

140

230

350

 

Max. trip time (ms)

80

140

200

320

500

 

Instantaneous Protection

Current Setting (A)
Accuracy: ±10%

Ii = In x...

2

3

4

6

8

10

12

15

off

MicroLogic 6.0P Trip Unit Ground-Fault Setting

Ground-Fault Pickup (A)
Accuracy: ±10%

Ig = ln x...

A

B

C

D

E

F

G

H

J

ln ≤ 400 A

0.3

0.3

0.4

0.5

0.6

0.7

0.8

0.9

1

400 A < ln ≤ 1200 A

0.2

0.3

0.4

0.5

0.6

0.7

0.8

0.9

1

ln > 1200 A

500

640

720

800

880

960

1040

1120

1200

Time Delay (s)
at 1 x In

Settings

I2t OFF

0.1

0.2

0.3

0.4

 

I2t ON

0.1

0.2

0.3

0.4

 

tg

Min. trip time (ms)

20

80

140

230

350

 

Max. trip time (ms)

80

140

200

320

500

 

Settings for Alarms for Other Protection Functions for MicroLogic 5.0P and 6.0P Trip Units

  Threshold Time Delay

Current

Current Imbalance

0.05 to 0.6 x Imax

1 to 40 s

Maximum Current

Imax: Ia, Ib, Ic, In, Ig

0.2 to 1.0 x In

15 to 1500 s

Voltage

Voltage Imbalance

0.02 to 0.3 x Vn

1 to 40 s

Minimum Voltage

Vmin

100 to 725 V (phase total)

0.25 to 0.5 s

Maximum Voltage

Vmax

100 to 1200 V (between phases)

0.20 to 5.0 s

Power

Maximum Power

Pmax

5 to 500 kW

0.2 to 20 s

Reverse Power

Pr

0.02 to 0.2 x Pn

0.5 to 20 s

Frequency

Minimum Frequency

Fmin

45 to 65 Hz

0.2 to 5 s

Maximum Frequency

Fmax

45 to 540 Hz

0.2 to 5 s

Phase

Sequence

ØA-ØB-ØC or ØA-ØC-ØB

Instantaneous

Load-Shedding Settings for Current and Power Metering for MicroLogic 5.0P and 6.0P Trip Units

Pick-Up

Drop-Out

Threshold

Time Delay

Threshold

Time Delay

Current

I

0.5 to 1.0 x Ir per phase

20% to 80% x tr

0.3 to 1.0 x Ir per phase

10 to 600 s

Power

P

200 kW to 10 MW

10 to 3600 s

100 kW to 10 MW

10 to 3600 s

Trip and Alarm Histories

The last ten trips and ten alarms are recorded in two separate history files that can be displayed on the screen (sample displays are shown to the right). The following information is contained in these files:


Trip History

Type of fault

Date and time of fault

Interrupted current

Contact wear


Alarm History

Type of alarm

Date and time of the alarm

Values measured at the time of the alarm

Power Trip Unit Metering

Current Metering

Maximum Current

Voltage Metering

Power Metering

Frequency

Power Demand

The MicroLogic P trip unit calculates in real time all electrical values V, A, W, VAR, VA, Wh, VARh, VAh, Hz, power factor, and crest factor. The MicroLogic P trip unit also calculates demand current and demand power over an adjustable time period.

Real-Time Metering: The value displayed on the screen is refreshed every second. Minimum and maximum measurement values are stored in memory.

Type of Measurement

Unit of Measurement

Measurement Source

Current

IRMS

A

ØA, ØB, ØC or N

IAVERAGE

A

(ØA + ØB + ØC)/3

IPEAK/Ö2

A

ØA, ØB, ØC or N

Voltage

VRMS

V

(ØA–ØB),. ØB–ØC) and (ØC–ØA)

VRMS

V

(ØA–N), (ØB–N) and ØC–N)

VIMBALANCE

%

VRMS

Power

P, Q and S

W, VAR, VA

Total

EP, EQ and ES

Wh, VARh, VAh

Total

Power factor

Total

Frequency

F

Hz

50/60

Demand Metering: The demand is calculated over a fixed or sliding time window that can be programmed from five to sixty minutes. Depending on the contract signed with the power supplier, specific programming makes it possible to avoid or minimize the cost of overrunning the subscribed power. Maximum demand values are systematically stored and time stamped.

Type of Measurement

Unit of Measurement

Measurement Source

Current

IDEMAND

A

ØA, ØB, ØC or N

Power

P, Q and SDEMAND

W, VAR, VA

Total

Power Trip Units Communication Network

Four wire Modbus, RTU, RS485—The communication network may be used to:

  • Remotely read parameters for the protection functions.

  • Transmit all the measurements and calculated values.

  • Signal the causes of tripping and alarms.

  • Consult the history files and the maintenance indicator record.

In addition, an event log of the last 100 events and a maintenance record, which is stored in the trip unit memory but not available locally, may be accessed via the communication network.

The Modbus communication system is compatible with PowerLogic™ System Manager™ (SMS) software.

Power Trip Unit Event Log

The event log may be accessed by a remote computer via the communication network. All events are time stamped and include:

  • Trips

  • Beginning and end of alarms

  • Modifications to settings and parameters

  • Loss of time

  • Overrun of wear indicators

  • Test kit connections

  • Counter resets

  • System faults (thermal self-protection, major fault and minor fault alarms)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.