0613CT0001

EcoStruxure Power Commission Tool

EcoStruxure Power Commission Tool Introduction

The EcoStruxure Power Commission Tool engineering tool is a software application that helps the user to manage a project as part of designing, testing, site commissioning, and maintenance of the project life cycle. It enables the user to prepare the settings of the devices offline (without connecting to the device) and configure them when connected with the devices. It also provides other value-added features for the user to manage the project such as: safe repository in cloud, attach artifacts to each device or at the project level, organize devices in switchboard, manage a hierarchical structure of the installation, etc.

Compatible Devices (Configuration and Device Management)

The EcoStruxure Power Commission engineering tool is compatible with the following devices:

  • ComPacT NSX100-630 (IEC) circuit breakers

  • PowerPacT (UL) circuit breakers

  • ComPacT NS630b-3200 (IEC) circuit breakers

  • MasterPacT NT/NW (IEC and UL) circuit breakers

  • Compatible devices (Device Management in the project)

  • Switches (ComPacT NSX, MasterPacT & PowerPacT Family)

  • Third party devices

References:

The EcoStruxure Oiwer Cimmission software package can be downloaded from our website:

www.schneider-electric.com

EcoStruxure Power Commission Tool Features

The EcoStruxure Power Commission Tool includes the Schneider Electric customer engineering tools such as the Remote Setting Utility (RSU) and Remote Control Utility (RCU) with additional features.

The EcoStruxure Power Commission Tool supports the connection of Schneider Electric communicable devices to:

  • create projects by device discovery, selection of devices, and importing a Bill of Material (BOM)

  • monitor the status of protection and I/O status

  • read information (alarms, measurements, parameters)

  • check protection discrimination between two devices

  • upload and download of configuration or settings in batch mode to multiple devices.

  • carry out commands and tests

  • generate and print a device settings report and communication test report

  • manage multiple devices with a electrical and communication hierarchy model

  • manage artifacts (project documents)

  • check consistency in settings between devices on a communication network

  • compare configuration settings between PC and device (online)

  • download latest firmware

The EcoStruxure Power Commission Tool enables the user to access the advanced features of the software once the project is saved in the Schneider Electric cloud.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.