0613CT0001

Ammeter (A) Trip Unit without 24 Vdc Power Supply at F1 and F2

Sensor Plug Value (In)

Minimum Ground-Fault Pickup

100–250 A

30% of sensor rating

400–1200 A

20% of sensor rating 1600–6300 A

1600–6300 A

500 A

  • Provides fault protection for LSIG functions.

  • Provides LED trip indication (powered by an onboard battery).

  • All display functions and trip unit features power-up with current flow on one phase greater than or equal to the values in the table to the left.

  • Ground-fault push-to-trip button works for testing ground fault with current flow on one phase greater than or equal to the values shown in the following table.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.