0613CT0001

Power (P) and Harmonic (H) Trip Unit with 24 Vdc Power Supply at F1 and F2

  • Provides all of the above.

  • LCD display and backlight are functional.

  • Ground-fault push-to-trip button works for testing ground fault.

  • All metering, monitoring, and history logs are functional.

  • Communications from trip unit to M2C and M6C programmable contact modules are powered by a 24 Vdc supply at F1 and F2. M6C also requires a 24 Vdc external power supply.

  • Modbus communications—also requires a separate 24 Vdc power supply for the circuit breaker communications module.

NOTE: Ground-fault push-to-trip button will also be functional if a service interface, a hand-held test kit, or a full-function test kit is powering the trip unit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.