0613CT0001

Measurement Function

Measurement Function

Instantaneous RMS Measurements

The MicroLogic trip unit continuously displays the RMS value of the highest current of the three phases and neutral (Imax). The navigation buttons can be used to scroll through the main measurements.

In the event of a fault trip, the trip cause is displayed.

The MicroLogic A trip unit measures phase, neutral, and ground fault currents.

MicroLogic P/H trip units offer voltage, power, power factor, frequency, and cos ? in addition to the measurements provided by MicroLogic A trip units.

Maximum / Minimum Ammeter

Every instantaneous measurement provided by MicroLogic A trip units can be associated with a maximum/minimum ammeter. The maximum for the highest current of the three phases, neutral, and demand current can be reset using the FDM display unit or the communication system.

Energy Metering

The MicroLogic P/H trip units also measures the energy consumed since the last reset of the meter. The active energy meter can be reset using the MicroLogic trip unit keypad, the FDM display unit, or the communication system.

Demand and Maximum Demand Values

MicroLogic P/H trip units also calculate demand current and power values. These calculations can be made using a block or sliding interval that can be set from five to sixty minutes in steps of one minute. The window can be synchronised with a signal sent through the communication system. Whatever the calculation method, the calculated values can be recovered on a PC through the communication network.

Ordinary spreadsheet software can be used to provide trend curves and forecasts based on this data. They provide a basis for load shedding and reconnection operations used to adjust consumption to the subscribed power.

Power Quality

The MicroLogic H trip unit calculates power quality indicators taking into account the presence of harmonics up to the fifteenth harmonic, including the total harmonic distortion (THD) of current and voltage.

MicroLogic A/P/H Trip Units Integrated Power Meter Functions

MicroLogic A/P/H Integrated Power Meter Functions

Type

Display

MicroLogic LCD

FDM Display

Display of protection settings

Pick-ups (A) and delays

All settings can be displayed

Ir, tr, Isd, tsd, Ii, Ig, tg

A/P/H

X

Measurements

Instantaneous rms measurements

Currents (A)

Phases and neutral

IA, IB, IC, IN

A/P/H

X

X

Average of phases

Iavg = (IA + IB + IC) / 3

A/P/H

X

Highest current of the 3 phases and neutral

Imax of IA, IB, IC, IN

A/P/H

X

X

Ground fault (MicroLogic 6)

% Ig (pick-up setting)

A/P/H

X

X

Current unbalance between phases

% Iavg

P/H

X

Voltages (V)

Phase-to-phase

VAB, VBC, VCA

P/H

X

X

Phase-to-neutral

VAN, VBN, VCN

P/H

X

X

Average of phase-to-phase voltages

Vavg = (VAB + VBC + VCA) / 3

P/H

X

Average of phase-to-neutral voltages

Vavg = (VAN + VBN + VCN) / 3

P/H

X

Ph-Ph and Ph-N voltage unbalance

% Vavg

P/H

X

Phase sequence

ABC, ACB

P/H

X

X*

Frequency (Hz)

Power system

f

P/H

X

X

Power

Active (kW)

P, total
P, per phase

P/H
P/H

X
X

X
X

Reactive (kVAR)

Q, total
Q, per phase

P/H
P/H

X
X

X
X

Apparent (kVA)

S, total
S, per phase

P/H
P/H

X
X

X
X

Power Factor

PF, total
PF, per phase

P/H
P/H

X
X

X
X

Cos φ

Cos φ, total
Cos φ, per phase

P/H
P/H

X
X

X
X

Maximum/Minimum Ammeter

Associated with instantaneous rms measurements

Reset using the FDM display unit and MicroLogic keypad

A/P/H

X

X

Energy Metering

Energy

Energy Active (kW), reactive (kVARh), apparent (kVAh)

Total since last reset

P/H

X

X

Demand and Maximum Demand Values

Demand Current (A)

Phases and neutral P

Present value on the selected window
Maximum demand since last reset

P/H
P/H

X
X

X
X

Demand Power

Active (kWh), reactive (kVAR), apparent (kVA)

Present value on the selected window
Maximum demand since last reset

P/H
P/H

X
X

X
X

Calculation Window

Sliding, fixed or com-synchronised

Adjustable from 5 to 60 minutes in 1 minute steps*

P/H

Power Quality

Total Harmonic Distortion (%)

Of voltage with respect to rms value

THDU,THDV of the Ph-Ph and Ph-N voltage

H

X

X

Of current with respect to rms value

THDI of the phase current

H

X

X

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.