0613CT0001

Power Meter Functions

In addition to protection functions, MicroLogic A/P/H trip units offer all the functions of Power Meter products as well as operating assistance for the circuit breaker.

MicroLogic A/P/H trip unit measurement functions are made possible by the MicroLogic trip unit’s intelligence and the accuracy of the sensors. They are handled by a microprocessor that operates independent of protection functions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.