0613CT0001

Energy Management Using the Enerlin’X System

Use the Enerlin’X communication system to connect a building to real savings in three steps:

A. Measure

  • Embedded and stand-alone metering and control

B. Connect

  • Integrated communication interfaces

  • Ready to connect to energy management platforms

C. Save

  • Data-driven energy efficiency actions

  • Real-time monitoring and control

  • Access to energy and site information through on-line services

Measure

Enerlin’X communication systems mean visible information.

Grouping most of the electrical protection, command and metering components, the switchboards are now significant sources of data locally displayed and sent via communication networks.

Connect

Enerlin’X communication systems use reliable, simple-to-install-and-use displays, and Ethernet and Modbus interfaces. Information is safely transmitted through the most efficient networks:

  • Modbus SL inside switchboards, between components,

  • Ethernet, on cable or WiFi, inside the building and connecting switchboards and computers,

  • Ethernet or GPRS, for access to on-line services by Schneider Electric.

Energy experts, no matter where they are located, can now provide advise based on the updated data of the building.

Save

On-Site Real-Time Monitoring and Control

The FDM128 touch screen display connected to the Ethernet:

  • shows essential electrical information and alarms concerning the electrical network,

  • allows control (open, close, reset…) of various equipment.

The FDM128 touch screen provides real-time value checking and control, directly on the front panel of the main switchboard.

On a PC display with common browser:

  • shows monitoring web pages hosted into the local Ethernet interface,

  • alarm events generate automatic email notifications,

  • allows control (open, close, reset…) of various equipment.

The data is displayed graphically or recorded into files for optimizing the use of energy in the building.

As an example, the data can help validate the change of temperature settings, time scheduling in a Building Management System or other automated devices.

On-Line Energy Management Services

StruXureWare Energy Operation automates data collection using an open, scalable, and secure energy management information system.

With the help of the Schneider Electric energy management services team, data is turned into information to enable customers to understand their facilities’ performance on an ongoing basis.

Energy Operation leverages companies’ current investments in their existing systems, and can be used to communicate advanced results and performance to a broad audience for a shared understanding throughout an organization.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.