0613CT0001

Wiring Diagrams

Wiring Diagrams for MasterPacT NW Circuit Breakers

Wiring Diagrams for MasterPacT NW Circuit Breakers

Power

Trip Unit

Remote Operation

A—Do not remove factory-installed jumpers between Z3, Z4 and Z5 unless ZSI is connected.
B—Do not remove factory-installed jumper between T1 and T2 unless neutral CT is connected. Do not install jumper between T3 and T4.
C—For proper wiring of neutral CT, refer to Instruction Bulletin 48041-082-01 shipped with it.
D—24 Vdc power supply for trip unit must be separate and isolated from 24 Vdc power supply for communication modules.
E—When remote operation features are used, make sure there is a minimum of four seconds for the spring charging motor (MCH) to completely charge the circuit       breaker closing springs prior to actuating the shunt close (XF) device.

Markings for Push-In Type Terminals

Markings for Ring Terminals

Auxiliary Contacts

Cell Switches

Markings for Push-In Type Terminals

NOTE: Fixed-mounted circuit breaker does not have cell switches (CE, CD, CT).

Markings for Ring Terminals

NOTE: Fixed-mounted circuit breaker does not have cell switches (CE, CD, CT).

Wiring Diagrams for MasterPacT NT Circuit Breakers

Wiring Diagrams for Push-In Type Terminals

Power

Trip Unit

Remote Operation

A—Do not remove factory-installed jumpers between Z3, Z4 and Z5 unless ZSI is connected.

B—Do not remove factory-installed jumper between T1 and T2 unless neutral CT is connected. Do not install jumper between T3 and T4.

C—For proper wiring of neutral CT, refer to Instruction Bulletin 48041-082-01 shipped with it.

D—24 Vdc power supply for trip unit must be separate and isolated from 24 Vdc power supply for communication modules.

E—When remote operation features are used, make sure there is a minimum of four seconds for the spring charging motor (MCH) to completely charge the circui breaker closing springs prior to actuating the shunt close (XF) device.

Markings for Push-In Type Terminals

Auxiliary Contacts

Cell Switches

Markings for Push-In Type Terminals

Spring-Charging Motor

Additional Wiring Information for MasterPacT NW/NT Circuit Breakers

Alarm Contacts (OF1, OF2, OF3 and OF4 are standard equipment)

OF4
OF3
OF2
OF1

Open/Closed Circuit Breaker or Switch Position Contacts

OF24: Open/Closed Circuit Breaker or Switch Position Contact
or
EF24: Combined Connected and Closed Contact

 

OF23 or EF23

OF22 or EF22

OF21 or EF21

OF14 or EF14

OF13 or EF13

OF12 or EF12

OF22 or EF22

OF11 or EF11

Cradle Contacts

CD3
CD2
CD1

Disconnected Position Contacts

CE3
CE2
CE1

Connected Position Contacts

CT3
CT2
CT1

Test Position Contacts

or

 

or

CE6CE5CE4

Connected Position Contacts

CE9
CE8
CE7

Connected Position Contacts

 

or

CD6
CD5
CD4

Disconnected Position Contacts

Trip Unit

Basic

A

P

H

X

X

X

Com:

E1–E6 Communication

X

X

X

UC1:

Z1–Z5 Logical Selectivity

X

X

X

Z1–Z5 Logical Selectivity

X

X

X

Z1 = ZSI OUT

X

X

X

Z2 = ZSI OUT Source; Z3 = ZSI IN Source

X

X

X

Z4 = ZSI IN Short-Time Delay

X

X

X

Z5 = ZSI IN Ground Fault

X

X

X

UC3:

F2+, F1– 24 Vdc External Power Supply

X

X

External Neutral VN Plug

X

X

UC4

External Phase Voltage Sensing

X

X

M2C or M6C

Two Programmable Contacts (internal relay)

X

X

Six Programmable Contacts
(for connection to external M6C module)

Remote Operation

SDE2 or RES

Electrical Fault Alarm Contact

Remote Reset

SDE1

Electrical Fault Alarm Contact (standard)

MN or MX2

Undervoltage Trip Device

Additional Shunt Trip

MX1

Shunt Trip (standard or networked)

XF

Shunt Close (standard or networked)

PF

Ready-to-Close Contact

MCH

Spring-Charging Motor

NOTE: When communication version of the MX1 or XF coils are used, terminals (C3, A3) must be connected to line even if the communications module is not installed.
The bypass circuit through terminal C2/A2 is only momentary duty for 0.5 sec. For continuous duty, use the communications command.

Connection of the Communications Option

NOTE: A recommended wiring schematic for the communicating style shunt trip or shunt close coils is shown below.

A2 can cause the shunt trip or shunt close to not work properly. The best way to control the induced voltages is keep the circuit to terminal C2 and A2 as short as possible. If it is impossible to keep the circuit less than 10 feet (3 m), use an interposing relay near terminal C2 or A2

A—24 Vdc power supply for trip unit must be separate and isolated from 24 Vdc power supply for communication modules.

B—Refer to instructions bulletin 48041-082 included with neutral CT for proper wiring.

NOTE: Fixed-mounted circuit breaker does not have cell switches (CE, CD, CT).

Wiring Diagrams for the COM Option

Wiring of the I/O Modules

See Connection of the Communications Option, page 125.

Wiring of the COM Option (Modbus BCM ULP and CCM Modules

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.