Schematics with ComPacT NSX Circuit Breakers
General Description
Depending on the configuration of the ComPacT NSX circuit breaker, connect the IFE communication interface to the circuit breaker using one of the following configurations:
-
Connection of the IFE communication interface to the MicroLogic 5, 6 or 7 trip unit
-
Connection of the IFE communication interface to the BSCM Modbus SL/ULP module
-
Connection of the IFE communication interface to the BSCM Modbus SL/ULP module and to the MicroLogic 5, 6 or 7 trip unit
For more information, refer to DOCA0093•• ULP System User Guide.
ULP Connection
All connection configurations require the NSX cord or the insulated NSX cord.
DANGER |
|---|
|
hazard of electric shock, explosion or arc flash
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
Connection of the IFE Communication Interface to the MicroLogic 5, 6 or 7 Trip Unit
Connection of the IFE Communication Interface to the BSCM Modbus SL/ULP Module
Connection of the IFE Communication Interface to the BSCM Modbus SL/ULP Module and to the MicroLogic 5, 6 or 7 Trip Unit
Connection of the IFE Communication Interface to a Circuit Breaker for System Voltage Greater Than 480 Vac or 480 Vdc
DANGER |
|---|
|
hazard of electric shock, explosion or arc flash
Failure to follow these instructions will result in death or serious injury.
|
DANGER