List of IO Module Commands
List of Commands
There are two types of command:
-
generic commands which work independently of the application selected.
-
application commands which are dedicated to an application. A command is only valid if the related application is configured.
The following table lists the available IO module commands, their corresponding application, command codes and user profiles. Follow the command execution procedures.
|
Application |
Command |
Command code |
User profile |
|---|---|---|---|
|
Generic |
1672 |
Administrator or Operator |
|
|
Generic |
41099 |
Administrator or Operator |
|
|
Generic |
41100 |
Administrator or Operator |
|
|
Generic |
41102 |
Administrator or Operator |
|
|
Generic |
42890 |
Administrator or Operator |
|
|
Cradle and drawer management |
41352 |
Administrator or Operator |
|
|
Cradle and drawer management |
41353 |
Administrator or Operator |
|
|
Light control |
42120 |
Administrator or Operator |
|
|
Load control |
42376 |
Administrator or Operator |
|
|
Pulse counter management |
42888 |
Administrator or Operator |
|
|
Cooling system |
42889 |
Administrator or Operator |
IO Module Error Codes
The error codes generated by the IO module are the generic error codesResult of the Command.