Write Protection
General Description
WARNING |
|---|
|
HAZARD OF NUISANCE TRIPPING OR FAILURE TO TRIP
Protection setting adjustments must be done by qualified
electrical personnel.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Remote modifications of Modbus registers can either be dangerous to personnel near the circuit breaker or can cause equipment damage if the protection settings are altered. Therefore, remote control commands are hardware protected and software protected.
Software Protection
To prevent an inadvertent change to the MicroLogic configuration, remote modifications of the Modbus registers are protected by both of the following:
-
a robust data structure and a set of dedicated Modbus registers
-
a user profile password scheme
This combination is called the command interface. Failure to conform to these results in an error code and the operation is not performed. The hardware protection has always precedence over the software protection.
WARNING