Measurement Configuration Commands
Set Up ENVT Presence
The user can read the ENVT (External Neutral Voltage Tap) presence parameters at register 3314. See System Type.
To set up ENVT presence, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
46472 |
Command code = 46472 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
0 = ENVT is not present. 1 = ENVT is present. |
Reset Minimum/Maximum
The reset minimum/maximum command resets the minimum values of real-time measurements (registers 1300 to 1599) and the maximum values of real-time measurements (registers 1600 to 1899). See Minimum/Maximum Values of Real-Time Measurements.
The reset minimum/maximum command resets the energy measurements (registers 2000 to 2025). See Energy Measurements.
The reset minimum/maximum command resets the peak demand measurements (registers 2200 to 2237). See Demand Measurements.
The user can read the minimum and maximum values of current, voltage, and frequency measurements and the corresponding dates from registers 29780 to 29827. See Minimum/Maximum V12 Voltage Measurements.
The user can read the dates of the reset minimum/maximum command from registers 2900 to 2929. See Minimum/Maximum Measurements Reset Time.
To reset minimum/maximum values of measurements, the user must set up the command registers as follows:
|
Address |
Register |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
INT16U |
46728 |
– |
Command code = 46728 |
|
0x1F40 |
8001 |
INT16U |
12 |
– |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
INT16U |
5121 |
– |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
INT16U |
1 |
– |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
OCTET STRING |
– |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
INT16U |
– |
– |
Reset minimum/maximum of metering variables:
|
|
0 |
Reset minimum/maximum current (I1, I2, I3, IN, Imax, Ig, IΔn, Iavg, and Iunbal) |
||||
|
1 |
Reset minimum/maximum voltage (V12, V13, V23, V1N, V2N, V3N, VavgL-L, VavgL-N, and Vunbal) |
||||
|
2 |
Reset minimum/maximum power (active power, reactive power, apparent power, and distortion power) |
||||
|
3 |
Reset minimum/maximum power factor and cosϕ |
||||
|
4 |
Reset minimum/maximum total harmonic distortion (THD) |
||||
|
5 |
Reset peak of current demand |
||||
|
6 |
Reset peak of active power, reactive power, and apparent power demand |
||||
|
7 |
Reset minimum/maximum frequency |
||||
|
8 |
Reset minimum/maximum thermal image (motor application only) |
||||
|
9 |
Reset energy (active, reactive, apparent) |
||||
|
10–15 |
Reserved |
Start/Stop Synchronization
The start/stop synchronization command is used to start or stop the calculation of the current or power demand. The first command starts the calculation, the next command updates the value of current or power demand, and then restarts the calculation. The time period between 2 commands must be less than 1 hour.
To start/stop synchronization, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
46729 |
Command code = 46729 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
– |
Start/stop synchronization = 1 |
Power Flow Sign Configuration
The user can read the power flow sign configuration at register 3316 Power Flow Sign.
To set the power flow sign parameters, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47240 |
Command code = 47240 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
Power flow sign: 0 = the active power flows from upstream (top) to downstream (bottom) (factory setting). 1 = the active power flows from downstream (bottom) to upstream (top). |
Power Factor Sign Configuration
The user can read the power factor sign configuration at register 3318 Power Factor Sign.
To set the power factor sign parameters, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47241 |
Command code = 47241 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–2 |
Sign convention for the power factor and the fundamental power factor (cosϕ): 0 = IEC convention 2 = IEEE convention (factory setting) |
Energy Accumulation Mode Configuration
The user can read the energy accumulation mode configuration at register 3324 Energy Accumulation Mode.
To set the energy accumulation mode parameters, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47242 |
Command code = 47242 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
Energy accumulation mode: 0 = absolute accumulation (factory setting) 1 = signed accumulation |
Current Demand Configuration
The user can read the duration of the current demand calculation window at register 3352 Demand Time.
The user can read the current demand parameters from registers 2200 to 2207 Current Demand.
To start current demand, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47243 |
Command code = 47243 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
Min |
INT16U |
5–60 |
Duration of the current demand calculation window, adjustable in steps of 1. The factory setting is 15 minutes (sliding). |
Power Demand Configuration
The user can read the power demand calculation method from registers 3354 to 3355 Demand Time.
The user can read the power demand parameters from registers 2224 to 2237 Active Power Demand.
To start power demand, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47244 |
Command code = 47244 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
14 |
Number of parameters (bytes) = 14 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
Min |
INT16U |
0–5 |
Power demand calculation method (window type): 0 = sliding 2 = fixed 5 = synchronized to communication The factory setting is 0 (sliding). |
|
0x1F46 |
8007 |
– |
Min |
INT16U |
5–60 |
Duration of the power demand calculation window, adjustable in steps of 1. The factory setting is 15 minutes. |
Set Up Nominal Voltage Vn Display
The user can read the nominal voltage at register 9616 Nominal Voltage.
To set the nominal voltage Vn display parameters, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47245 |
Command code = 47245 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
V |
INT16U |
0–65535 |
Nominal voltage Vn (factory setting = 400 V) |
Phase Rotation Configuration
The user can read the phase rotation at register 3315.
To set the phase rotation parameters, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47246 |
Command code = 47546 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
Phase rotation: 0 = I1, I2, I3 (factory setting) 1 = I1, I3, I2 |