Event History
General Description
The event history registers describe the last 100 events. The event history format corresponds to a series of 100 records. Each record is composed of 5 registers describing one event.
A read request of 5x(n) registers is necessary to read the last n event records, where 5 is the number of registers for each event record.
For example, a read request of 5x3 = 15 registers is necessary to read the last 3 event records of the event history:
-
The first five registers describe the first event record (most recent event).
-
The next five registers describe the second event record.
-
The last five registers describe the third event record.
There are two event histories, 1 per IO module.
|
IO Module |
Address |
Register |
Description |
|---|---|---|---|
|
IO 1 |
0x39A7–0x39AB |
14760–14764 |
Event record 1 (most recent event record) |
|
0x39AC–0x39B0 |
14765–14769 |
Event record 2 |
|
|
0x39A7+5x(n-1)–0x39AB+5x(n-1) |
14760+5x(n-1)–14764+5x(n-1) |
Event record n |
|
|
0x3B96–0x3B9A |
15255–15259 |
Event record 100 |
|
|
IO 2 |
0x455F–0x4563 |
17760–17764 |
Event record 1 (most recent event record) |
|
0x4564–0x4568 |
17765–17769 |
Event record 2 |
|
|
0x455F+5x(n-1)–0x4563+5x(n-1) |
17760+5x(n-1)–17764+5x(n-1) |
Event record n |
|
|
0x474E–0x4752 |
18255–18259 |
Event record 100 |
Event Record
A block request of five registers is necessary to read an event record.The order and the description of the event record registers of IO 2 are the same as those of IO 1:
|
Event Record 1 (Most Recent Event Record) |
||||
|---|---|---|---|---|
|
Register |
Address |
RW |
Type |
Description |
|
0x39A7 |
14760 |
R |
INT16U |
|
|
0x39A8– 0x39AA |
14761– 14763 |
R |
ULP DATE |
Date and time of the event |
|
0x39AB |
14764 |
R |
INT16U |
Event type MSB = 0 (reserved) Event occurrence: LSB = 1 Event completion: LSB = 2 |
Alarm Definition
Alarms are specific events that need to be reset.
The reset mode of an alarm can be:
-
automatic: the alarm is reset automatically when the alarm is no more active.
-
manual: the alarm is reset manually with the Test/Reset pushbutton located on the front face of the IO module and when the alarm is no more active.
-
remote: the alarm is reset remotely with the Reset command sent via the communication and when the alarm is no more active.
Each alarm has a priority level that manages the alarm display on the FDM121 display:
-
no priority = N/A (not affected)
-
low priority = 1. No alarm display on the FDM121 display
-
medium priority = 2. The FDM121 display LED is steady ON.
-
high priority = 3. The FDM121 display LED blinks and a pop-up screen informs that the alarm has occurred.