Digital Outputs
Digital Output Register Mapping
Each digital output description is made up of 60 registers. The order and the description of the digital outputs 2 and 3 are the same as those of digital output 1.
|
IO Module |
Digital Output Number |
Digital Output Addresses |
Digital Output Registers |
|---|---|---|---|
|
IO 1 |
O1 |
0x3849–0x3884 |
14410–14469 |
|
O2 |
0x3885–0x38C0 |
14470–14529 |
|
|
O3 |
0x38C1–0x38FC |
14530–14589 |
|
|
IO 2 |
O1 |
0x4401–0x443C |
17410–17469 |
|
O2 |
0x443D–0x4478 |
17470–17529 |
|
|
O3 |
0x4479–0x44B4 |
17530–17589 |
Digital Output 1 Registers of IO 1
The order and the description of the digital output 1 registers of IO 2 are the same as those of IO 1:
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3849 |
14410 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14411:
|
|
0x384A |
14411 |
R-WC |
– |
INT16U |
– |
0 |
Reserved |
|
1 |
Digital output status:
|
||||||
|
R |
2 |
Digital output forced status:
|
|||||
|
3–15 |
Reserved |
||||||
|
0x384B–0x384E |
14412–14415 |
R |
– |
DATETIME |
– |
– |
Timestamp for the last output transition:
|
|
0x384F–0x3850 |
14416–14417 |
– |
– |
– |
– |
– |
Reserved |
|
0x3851–0x3852 |
14418–14419 |
R |
– |
INT32U |
1-4294967294 |
– |
Output counter This counter increments for each rising edge of the output. |
|
0x3853–0x3856 |
14420–14423 |
R |
– |
DATETIME |
– |
– |
Timestamp of the last reset for the output counter |
|
0x3857–0x386E |
14424–14447 |
R |
– |
OCTET STRING |
– |
– |
Digital output identification coded over 45 ASCII characters |
|
0x386F |
14448 |
R |
– |
INT16U |
0–2 |
– |
Output operating mode(1):
|
|
0x3870 |
14449 |
R |
s |
INT16U |
0–65534 |
– |
On time for time delayed non-latching mode value(1) The time for the output to remain energized when the output is in time delayed non-latching mode (Factory setting = 0) |
|
0x3871 |
14450 |
R |
– |
INT16U |
0–1 |
– |
Output contact type(1):
|
|
0x3872 |
14451 |
R |
– |
INT16U |
0–2 |
– |
Indicates On/Off state of the discrete output when any fall back condition occurs(1):
|
|
0x3873–0x3874 |
14452–14453 |
R |
– |
INT32U |
1-4294967294 |
– |
Output counter threshold value(1) Factory setting = 5000 |
|
0x3875 |
14454 |
R-WC |
– |
INT16U |
0–2 |
– |
Simple command for output(1):
Valid if simple commands are enabled(2). |
|
0x3876–0x3884 |
14455–14469 |
– |
– |
– |
– |
– |
Reserved |
|
(1) Value set using EcoStruxure Power Commission software. (2) Simple commands are enabled by factory setting. The simple commands can be disabled by using the command Enable/Disable commands. |
|||||||