Earth-Leakage Test History
General Description
The earth-leakage test history registers describe the last 10 earth-leakage tests performed on a MicroLogic 7 trip unit. The earth-leakage test history format corresponds to a series of 10 records. Each record is composed of 5 registers describing one earth-leakage test.
The earth-leakage test history registers return 32768 (0x8000) when they are not used.
Earth-Leakage Test Number
A read request of 5 x n registers is necessary to read the last n earth-leakage test records, where 5 is the number of registers for each earth-leakage test record.
For example, a read request of 5 x 2 = 10 registers is necessary to read the last 2 earth-leakage test records of the earth-leakage test history:
-
The first 5 registers describe the first earth-leakage test record (most recent earth-leakage test).
-
The last 5 registers describe the second earth-leakage test record.
|
Address |
Register |
Description |
|---|---|---|
|
0x7593–0x7597 |
30100-30104 |
Earth-leakage test record (most recent earth-leakage test) |
|
0x7598–0x759C |
30105–30109 |
Earth-leakage test record 2 |
|
0x759D–0x75A1 |
30110–30114 |
Earth-leakage test record 3 |
|
0x75A2–0x75A6 |
30115–30119 |
Earth-leakage test record 4 |
|
0x75A7–0x75AB |
30120–30124 |
Earth-leakage test record 5 |
|
0x75AC–0x75B0 |
30125–30129 |
Earth-leakage test record 6 |
|
0x75B1–0x75B5 |
30130–30134 |
Earth-leakage test record 7 |
|
0x75B6–0x75BA |
30135–30139 |
Earth-leakage test record 8 |
|
0x75BB–0x75BF |
30140–30144 |
Earth-leakage test record 9 |
|
0x75C0–0x75C4 |
30145–30149 |
Earth-leakage test record 10 (oldest earth-leakage test) |
Earth-Leakage Test Record
A read request of 5 registers is necessary to read a earth-leakage test record.
The order and the description of the earth-leakage test record registers are the same as that of the earth-leakage test record 1:
|
Earth-Leakage Test Record 1 (Most Recent Earth-Leakage Test) |
|||||||
|---|---|---|---|---|---|---|---|
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|
0x7593 |
30100 |
R |
1 |
– |
INT16U |
0–65535 |
Earth-leakage test code (see next section.) |
|
0x7594– 0x7596 |
30101– 30103 |
R |
– |
– |
ULP DATE |
– |
Date and time of earth-leakage test. Data Type: ULP DATE |
|
0x7597 |
30104 |
R |
– |
– |
INT16U |
0–1 |
Test status
|
Earth-Leakage Test Codes
|
Earth-Leakage Test Code |
Description |
|---|---|
|
5162 (0x142A) |
Earth-leakage test by button |
|
5163 (0x142B) |
Earth-leakage test by HMI |