Legacy Dataset Common Registers
Circuit Breaker Status Register
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EDF |
12000 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
X |
– |
Validity of each bit in the circuit breaker status register. |
|
0x2EE0 |
12001 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
X |
– |
Circuit breaker status register |
|
A/E |
A/E/P/H |
X |
0 |
OF status indication contact 0 = The circuit breaker is open. 1 = The circuit breaker is closed. |
||||||
|
A/E |
A/E/P/H |
X |
1 |
SD trip indication contact 0 = Circuit breaker is not tripped. 1 = Circuit breaker is tripped due to electrical fault, shunt trip or push-to-trip. Bit always equal to 0 for MasterPacT NT/NW and ComPacT NS circuit breakers with motor mechanism. |
||||||
|
A/E |
A/E/P/H |
X |
2 |
SDE fault trip indication contact 0 = Circuit breaker is not tripped on electrical fault. 1 = Circuit breaker is tripped due to electrical fault (including ground-fault test and earth-leakage test). |
||||||
|
– |
A/E/P/H |
X |
3 |
CH spring charged contact (only with MasterPacT) 0 = Spring discharged 1 = Spring charged Bit always equal to 0 for ComPacT NS circuit breaker. |
||||||
|
– |
– |
– |
4 |
Reserved |
||||||
|
– |
A/E/P/H |
X |
5 |
PF ready to close contact (only with MasterPacT) 0 = Not ready to close 1 = Ready to close Bit always equal to 0 for ComPacT NS circuit breaker. |
||||||
|
– |
A/E/P/H |
X |
6 |
Distinction between ComPacT NS and MasterPacT NT/NW 0 = ComPacT NS 1 = MasterPacT NT/NW |
||||||
|
– |
– |
– |
7–14 |
Reserved |
||||||
|
A/E |
– |
X |
15 |
Data availability If this bit is set at 1, all other bits of the register are not significant. |
IO Status Registers
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EE1 |
12002 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
X |
– |
Status IO 1 |
|
0 |
Input 1 status
|
|||||||||
|
1 |
Input 2 status
|
|||||||||
|
2 |
Input 3 status
|
|||||||||
|
3 |
Input 4 status
|
|||||||||
|
4 |
Input 5 status
|
|||||||||
|
5 |
Input 6 status
|
|||||||||
|
6 |
Output 1 status
|
|||||||||
|
7 |
Output 2 status
|
|||||||||
|
8 |
Output 3 status
|
|||||||||
|
9–14 |
Reserved |
|||||||||
|
15 |
Data availability If this bit is set at 1, all other bits of the register are not significant. |
|||||||||
|
0x2EE2 |
12003 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
X |
– |
Status IO 2 |
|
0 |
Input 1 status
|
|||||||||
|
1 |
Input 2 status
|
|||||||||
|
2 |
Input 3 status
|
|||||||||
|
3 |
Input 4 status
|
|||||||||
|
4 |
Input 5 status
|
|||||||||
|
5 |
Input 6 status
|
|||||||||
|
6 |
Output 1 status
|
|||||||||
|
7 |
Output 2 status
|
|||||||||
|
8 |
Output 3 status
|
|||||||||
|
9–14 |
Reserved |
|||||||||
|
15 |
Data availability If this bit is set at 1, all other bits of the register are not significant. |
Tripping Cause
The tripping cause register provides information about the cause of the trip for the standard protection functions. When a tripping cause bit is at 1 in the tripping cause register, it indicates that a trip has occurred and has not been reset.
-
For MicroLogic trip units for ComPacT NSX circuit breakers, the tripping cause bit is reset by pressing the OK key (keypad of the MicroLogic trip unit) twice (validation and confirmation).
-
For MicroLogic A/E/P/H trip units for MasterPacT NT/NW and ComPacT NS circuit breakers, the tripping cause bit is reset as soon as the circuit breaker is closed again.
-
For MicroLogic X control units for MasterPacT MTZ circuit breakers, the tripping cause bit is reset by pressing the test/reset button (located beside the trip cause LEDs on the MicroLogic X control unit). Press and hold the button for 3 to 15 seconds to reset all the trip causes.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EE3 |
12004 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
X |
– |
Tripping cause for the standard protection functions |
|
A/E |
A/E/P/H |
X |
0 |
Long-time protection Ir |
||||||
|
A/E |
P/H |
X |
1 |
Short-time protection Isd |
||||||
|
– |
A/E |
X |
1 |
Short-time protection Isd or Instantaneous protection Ii |
||||||
|
A/E |
P/H |
X |
2 |
Instantaneous protection Ii |
||||||
|
A/E |
A/E/P/H |
X |
3 |
Ground-fault protection Ig |
||||||
|
E |
A/P/H |
X |
4 |
Earth-leakage protection IΔn |
||||||
|
A/E |
A/E/P/H |
X |
5 |
Integrated instantaneous protection for:
|
||||||
|
A/E |
– |
X |
6 |
Internal failure (STOP) |
||||||
|
– |
A/E |
– |
Other protections or integrated instantaneous protection |
|||||||
|
– |
P/H |
– |
Internal failure (temperature) |
|||||||
|
– |
A/E/P/H |
– |
7 |
Internal failure (overvoltage) |
||||||
|
– |
P/H |
X |
8 |
Other protection (see register 12005) |
||||||
|
E |
– |
– |
9 |
Instantaneous with earth-leakage protection on the trip unit. |
||||||
|
E |
– |
– |
10 |
Unbalance motor protection |
||||||
|
E |
– |
– |
11 |
Jam motor protection |
||||||
|
E |
– |
– |
12 |
Underload motor protection |
||||||
|
E |
– |
– |
13 |
Long-start motor protection |
||||||
|
A/E |
– |
– |
14 |
Reflex tripping protection |
||||||
|
A/E |
A/E/P/H |
X |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EE4 |
12005 |
R |
– |
INT16U |
– |
– |
P/H |
X |
– |
Tripping causes for the advanced protection functions |
|
– |
P/H |
– |
0 |
Current unbalance |
||||||
|
– |
P/H |
– |
1 |
Overcurrent on phase 1 |
||||||
|
– |
P/H |
– |
2 |
Overcurrent on phase 2 |
||||||
|
– |
P/H |
– |
3 |
Overcurrent on phase 3 |
||||||
|
– |
P/H |
– |
4 |
Overcurrent on Neutral |
||||||
|
– |
P/H |
X |
5 |
Undervoltage |
||||||
|
– |
P/H |
X |
6 |
Overvoltage |
||||||
|
– |
P/H |
– |
7 |
Voltage unbalance |
||||||
|
– |
P/H |
– |
8 |
Overpower |
||||||
|
– |
P/H |
X |
9 |
Reverse power |
||||||
|
– |
P/H |
X |
10 |
Underfrequency |
||||||
|
– |
P/H |
X |
11 |
Overfrequency |
||||||
|
– |
P/H |
– |
12 |
Phase rotation |
||||||
|
– |
P/H |
– |
13 |
Load shedding based on current |
||||||
|
– |
P/H |
– |
14 |
Load shedding based on power |
||||||
|
– |
P/H |
X |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EE5– 0x2EE6 |
12006– 12007 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |
Overrun of the Protection Setpoints
The alarm setpoint registers provide information about overrun of the standard and advanced protection setpoints. A bit is at 1 once a setpoint overrun has occurred, even if the time delay has not expired.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EE7 |
12008 |
R |
– |
INT16U |
– |
A/E |
P/H |
– |
– |
Overrun of the standard protection setpoints |
|
A/E |
P/H |
– |
0 |
Long-time protection pick-up |
||||||
|
– |
– |
– |
1–14 |
Reserved |
||||||
|
A/E |
P/H |
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EE8 |
12009 |
R |
– |
INT16U |
– |
– |
P/H |
– |
– |
Overrun of the advanced protection setpoints |
|
– |
P/H |
– |
0 |
Current unbalance |
||||||
|
– |
P/H |
– |
1 |
Maximum current on phase 1 |
||||||
|
– |
P/H |
– |
2 |
Maximum current on phase 2 |
||||||
|
– |
P/H |
– |
3 |
Maximum current on phase 3 |
||||||
|
– |
P/H |
– |
4 |
Maximum current on the neutral |
||||||
|
– |
P/H |
– |
5 |
Minimum voltage |
||||||
|
– |
P/H |
– |
6 |
Maximum voltage |
||||||
|
– |
P/H |
– |
7 |
Voltage unbalance |
||||||
|
– |
P/H |
– |
8 |
Maximum power |
||||||
|
– |
P/H |
– |
9 |
Reverse power |
||||||
|
– |
P/H |
– |
10 |
Minimum frequency |
||||||
|
– |
P/H |
– |
11 |
Maximum frequency |
||||||
|
– |
P/H |
– |
12 |
Phase rotation |
||||||
|
– |
P/H |
– |
13 |
Load shedding based on the current |
||||||
|
– |
P/H |
– |
14 |
Load shedding based on the power |
||||||
|
– |
P/H |
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EE9 |
12010 |
R |
– |
INT16U |
– |
– |
P/H |
– |
– |
Continuation of the previous register |
|
– |
P/H |
– |
0 |
Ground-fault alarm |
||||||
|
E |
P/H |
– |
1 |
Earth-leakage alarm |
||||||
|
– |
– |
– |
2–14 |
Reserved |
||||||
|
– |
P/H |
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
Alarms
The alarm register provides information about the pre-alarms and the user-defined alarms. A bit is set to 1 once an alarm is active.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EEA |
12011 |
R |
– |
INT16U |
– |
A/E |
– |
X |
– |
Pre-alarm register |
|
A/E |
– |
X |
0 |
Long-time protection time pre-alarm (PAL Ir) |
||||||
|
E |
– |
– |
1 |
Earth-leakage protection pre-alarm (PAL IΔn) |
||||||
|
– |
– |
X |
Earth-leakage alarm(1) |
|||||||
|
A/E |
– |
– |
2 |
Ground-fault protection pre-alarm (PAL Ig) |
||||||
|
– |
– |
X |
Ground-fault alarm(2) |
|||||||
|
– |
– |
– |
3–14 |
Reserved |
||||||
|
A/E |
– |
X |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EEB |
12012 |
R |
– |
INT16U |
– |
A/E |
– |
– |
– |
Register of user-defined alarms |
|
A/E |
– |
– |
0 |
User-defined alarm 201 |
||||||
|
A/E |
– |
– |
1 |
User-defined alarm 202 |
||||||
|
A/E |
– |
– |
2 |
User-defined alarm 203 |
||||||
|
A/E |
– |
– |
3 |
User-defined alarm 204 |
||||||
|
A/E |
– |
– |
4 |
User-defined alarm 205 |
||||||
|
A/E |
– |
– |
5 |
User-defined alarm 206 |
||||||
|
A/E |
– |
– |
6 |
User-defined alarm 207 |
||||||
|
A/E |
– |
– |
7 |
User-defined alarm 208 |
||||||
|
A/E |
– |
– |
8 |
User-defined alarm 209 |
||||||
|
A/E |
– |
– |
9 |
User-defined alarm 210 |
||||||
|
– |
– |
– |
10–14 |
Reserved |
||||||
|
A/E |
– |
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EEC– 0x2EEE |
12013– 12015 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) Value available on MicroLogic 7.0 X control unit only when the Digital Module ANSI 51N/51G Ground-fault alarm is installed. (2) Value available on MicroLogic 2.0 X, 3.0 X, 5.0 X, and 6.0 X control units only when the Digital Module ANSI 51N/51G Ground-fault alarm is installed. |
||||||||||
Current
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2EEF |
12016 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
RMS current on phase 1: I1 |
|
0x2EF0 |
12017 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
RMS current on phase 2: I2 |
|
0x2EF1 |
12018 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
RMS current on phase 3: I3 |
|
0x2EF2 |
12019 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
RMS current on the neutral: IN (1) |
|
0x2EF3 |
12020 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
Maximum of I1, I2, I3, and IN |
|
0x2EF4 |
12021 |
R |
%Ig |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
Ground-fault current Ig (2) |
|
0x2EF5 |
12022 |
R |
%lΔn |
INT16U |
0–32767 |
E |
A/P/H |
X |
Earth-leakage current IΔn (3) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral current transformer (ENCT). (2) This value is only available:
(3) This value is only available:
|
|||||||||
Maximum Current Values
Maximum current values can be reset with the reset minimum/maximum command.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2EF6 |
12023 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
Maximum RMS current on phase 1: I1 |
|
0x2EF7 |
12024 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
Maximum RMS current on phase 2: I2 |
|
0x2EF8 |
12025 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
Maximum RMS current on phase 3: I3 |
|
0x2EF9 |
12026 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
Maximum RMS current on the neutral: IN (1) |
|
0x2EFA |
12027 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
Maximum RMS current out of the 4 previous registers |
|
0x2EFB |
12028 |
R |
%Ig |
INT16U |
0–32767 |
A/E |
A/E/P/H |
X |
Maximum ground-fault current Ig (2) |
|
0x2EFC |
12029 |
R |
%lΔn |
INT16U |
0–32767 |
E |
A/P/H |
X |
Maximum earth-leakage current (3) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral current transformer (ENCT). (2) This value is only available:
(3) This value is only available:
|
|||||||||
Voltage
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2EFD |
12030 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
RMS phase-to-phase voltage V12 |
|
0x2EFE |
12031 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
RMS phase-to-phase voltage V23 |
|
0x2EFF |
12032 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
RMS phase-to-phase voltage V31 |
|
0x2F00 |
12033 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
RMS phase-to-neutral voltage V1N (1) |
|
0x2F01 |
12034 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
RMS phase-to-neutral voltage V2N (1) |
|
0x2F02 |
12035 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
RMS phase-to-neutral voltage V3N (1) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral voltage transformer (ENVT). |
|||||||||
Frequency
When the MicroLogic trip unit cannot calculate the frequency, it returns Not applicable = 32768 (0x8000).
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F03 |
12036 |
R |
0.1 Hz |
INT16U |
400–600 |
E |
P/H |
X |
Frequency |
|
0x2F04 |
12037 |
R |
0.1 Hz |
INT16U |
400–600 |
E |
P/H |
X |
Maximum frequency (1) |
|
(1) This value can be reset with the reset minimum/maximum command. |
|||||||||
Power
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F05 |
12038 |
R |
0.1 kW |
INT16 |
-32767–+32767 |
E |
E/P/H |
X |
Active power on phase 1: P1 (1) (2) |
|
0x2F06 |
12039 |
R |
0.1 kW |
INT16 |
-32767–+32767 |
E |
E/P/H |
X |
Active power on phase 2: P2 (1) (2) |
|
0x2F07 |
12040 |
R |
0.1 kW |
INT16 |
-32767–+32767 |
E |
E/P/H |
X |
Active power on phase 3: P3 (1) (2) |
|
0x2F08 |
12041 |
R |
0.1 kW |
INT16 |
-32767–+32767 |
E |
E/P/H |
X |
Total active power: Ptot (2) |
|
0x2F09 |
12042 |
R |
0.1 kVAR |
INT16 |
-32767–+32767 |
E |
E/P/H |
X |
Reactive power on phase 1: Q1 (1) (2) |
|
0x2F0A |
12043 |
R |
0.1 kVAR |
INT16 |
-32767–+32767 |
E |
E/P/H |
X |
Reactive power on phase 2: Q2 (1) (2) |
|
0x2F0B |
12044 |
R |
0.1 kVAR |
INT16 |
-32767–+32767 |
E |
E/P/H |
X |
Reactive power on phase 3: Q3 (1) (2) |
|
0x2F0C |
12045 |
R |
0.1 kVAR |
INT16 |
-32767–+32767 |
E |
E/P/H |
X |
Total reactive power: Qtot (2) |
|
0x2F0D |
12046 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
E/P/H |
X |
Apparent power on phase 1: S1 (1) |
|
0x2F0E |
12047 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
E/P/H |
X |
Apparent power on phase 2: S2 (1) |
|
0x2F0F |
12048 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
E/P/H |
X |
Apparent power on phase 3: S3 (1) |
|
0x2F10 |
12049 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
E/P/H |
X |
Total apparent power: Stot |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral current transformer (ENCT). (2) The sign for the active and reactive power depends on the configuration of:
|
|||||||||
Energy
Energy is stored in big-endian format: the most significant register is transmitted first, the least significant second.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F11– 0x2F12 |
12050– 12051 |
R |
kWh |
INT32 |
-1 999 999 999– +1 999 999 999 |
E |
E/P/H |
X |
Active energy: Ep (1) |
|
0x2F13– 0x2F14 |
12052– 12053 |
R |
kVARh |
INT32 |
-1 999 999 999– +1 999 999 999 |
E |
E/P/H |
X |
Reactive energy: Eq (1) |
|
0x2F15– 0x2F16 |
12054– 12055 |
R |
kWh |
INT32U |
0–1 999 999 999 |
E |
P/H |
X |
Active energy counted positively: EpIn |
|
0x2F17– 0x2F18 |
12056– 12057 |
R |
kWh |
INT32U |
0–1 999 999 999 |
E |
P/H |
X |
Active energy counted negatively: EpOut |
|
0x2F19– 0x2F1A |
12058– 12059 |
R |
kVARh |
INT32U |
0–1 999 999 999 |
E |
P/H |
X |
Reactive energy counted positively: EqIn |
|
0x2F1B– 0x2F1C |
12060– 12061 |
R |
kVARh |
INT32U |
0–1 999 999 999 |
E |
P/H |
X |
Reactive energy counted negatively: EqOut |
|
0x2F1D–0x2F1E |
12062– 12063 |
R |
kVAh |
INT32U |
0–1 999 999 999 |
E |
E/P/H |
X |
Total apparent energy: Es |
|
0x2F1F– 0x2F20 |
12064– 12065 |
R |
kWh |
INT32U |
0–1 999 999 999 |
E |
– |
X |
Active energy counted positively (non-resettable): EpIn |
|
0x2F21– 0x2F22 |
12066– 12067 |
R |
kWh |
INT32U |
0–1 999 999 999 |
E |
– |
X |
Active energy counted negatively (non-resettable): EpOut |
|
0x2F23– 0x2F2E |
12068– 12079 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) This value is always positive with MicroLogic E trip units for MasterPacT NT/NW and ComPacT NS circuit breakers. |
|||||||||
Current Demand Values
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F2F |
12080 |
R |
A |
INT16U |
0–32767 |
E |
E/P/H |
X |
Current demand value on phase 1: I1 Dmd |
|
0x2F30 |
12081 |
R |
A |
INT16U |
0–32767 |
E |
E/P/H |
X |
Current demand value on phase 2: I2 Dmd |
|
0x2F31 |
12082 |
R |
A |
INT16U |
0–32767 |
E |
E/P/H |
X |
Current demand value on phase 3: I3 Dmd |
|
0x2F32 |
12083 |
R |
A |
INT16U |
0–32767 |
E |
E/P/H |
X |
Current demand value on the neutral: IN Dmd (1) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral current transformer (ENCT). |
|||||||||
Power Demand Values
-
For the block window, the demand value is updated at the end of the window.
-
For the sliding window,
-
If window duration is configured for less or equal to 15 minutes, the demand value is updated every 15 seconds
-
If window duration is configured for more than 15 minutes, the demand value is updated every 1 minute.
-
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F33 |
12084 |
R |
0.1 kW |
INT16U |
0–32767 |
E |
E/P/H |
X |
Total active power demand: P Dmd |
|
0x2F34 |
12085 |
R |
0.1 kVAR |
INT16U |
0–32767 |
E |
P/H |
X |
Total reactive power demand: Q Dmd |
|
0x2F35 |
12086 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
P/H |
X |
Total apparent power demand: S Dmd |
|
0x2F36– 0x2F38 |
12087– 12089 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
Maximum Voltage Values
Maximum voltage values can be reset with the reset minimum/maximum command.
Register = 0 if the voltage < 25 V.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F39 |
12090 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
Maximum RMS phase-to-phase voltage V12 |
|
0x2F3A |
12091 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
Maximum RMS phase-to-phase voltage V23 |
|
0x2F3B |
12092 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
Maximum RMS phase-to-phase voltage V31 |
|
0x2F3C |
12093 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
Maximum RMS phase-to-neutral voltage V1N (1) |
|
0x2F3D |
12094 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
Maximum RMS phase-to-neutral voltage V2N (1) |
|
0x2F3E |
12095 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
X |
Maximum RMS phase-to-neutral voltage V3N (1) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral voltage transformer (ENVT). |
|||||||||
Power Factor
The sign for the fundamental power factor (cosϕ) depends on the MicroLogic configuration.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F3F |
12096 |
R |
0.01 |
INT16 |
-100– +100 |
E |
E/P/H |
X |
Power factor on phase 1: PF1 (1) |
|
0x2F40 |
12097 |
R |
0.01 |
INT16 |
-100– +100 |
E |
E/P/H |
X |
Power factor on phase 2: PF2 (1) |
|
0x2F41 |
12098 |
R |
0.01 |
INT16 |
-100– +100 |
E |
E/P/H |
X |
Power factor on phase 3: PF3 (1) |
|
0x2F42 |
12099 |
R |
0.01 |
INT16 |
-100– +100 |
E |
E/P/H |
X |
Total power factor: PF |
|
0x2F43 |
12100 |
R |
0.01 |
INT16 |
-100– +100 |
E |
H |
X |
Fundamental power factor on phase 1: cosϕ1 (1) |
|
0x2F44 |
12101 |
R |
0.01 |
INT16 |
-100– +100 |
E |
H |
X |
Fundamental power factor on phase 2: cosϕ2 (1) |
|
0x2F45 |
12102 |
R |
0.01 |
INT16 |
-100– +100 |
E |
H |
X |
Fundamental power factor on phase 3: cosϕ3 (1) |
|
0x2F46 |
12103 |
R |
0.01 |
INT16 |
-100– +100 |
E |
H |
X |
Total fundamental power factor: cosϕ |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral voltage transformer (ENVT). |
|||||||||
Total Harmonic Distortion (THD)
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F47 |
12104 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of V12 compared to the fundamental |
|
0x2F48 |
12105 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of V23 compared to the fundamental |
|
0x2F49 |
12106 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of V31 compared to the fundamental |
|
0x2F4A |
12107 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of V1N compared to the fundamental (1) |
|
0x2F4B |
12108 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of V2N compared to the fundamental (1) |
|
0x2F4C |
12109 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of V3N compared to the fundamental (1) |
|
0x2F4D |
12110 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of I1 compared to the fundamental |
|
0x2F4E |
12111 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of I2 compared to the fundamental |
|
0x2F4F |
12112 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of I3 compared to the fundamental |
|
0x2F50 |
12113 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
X |
Total harmonic distortion of total current compared to the fundamental |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral voltage transformer (ENVT). |
|||||||||
Counters
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2F7F |
12160 |
R |
– |
INT16U |
0–32766 |
A/E |
A/E/P/H |
X |
Trip counter |
|
0x2F80 |
12161 |
R |
– |
INT16U |
0–32766 |
A/E |
A/E/P/H |
X |
Counter of alarms with priority level = 3 (high) |
|
0x2F81 |
12162 |
R |
– |
INT16U |
0–32766 |
A/E |
A/E/P/H |
X |
Counter of alarms with priority level = 2 (medium) |
|
0x2F82 |
12163 |
R |
– |
INT16U |
0–32766 |
A/E |
A/E/P/H |
X |
Counter of alarms with priority level = 1 (low) |
Miscellaneous
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F83 |
12164 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
X |
– |
Validity of the breaker close inhibit |
|
0 |
Validity of the breaker close inhibit by IO module |
|||||||||
|
1 |
Validity of the breaker close inhibit by remote controller |
|||||||||
|
2–15 |
Reserved |
|||||||||
|
0x2F84 |
12165 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
X |
– |
Status of the breaker close inhibit |
|
0 |
Status of the breaker close inhibit by IO module |
|||||||||
|
1 |
Status of the breaker close inhibit by remote controller |
|||||||||
|
2–15 |
Reserved |
|||||||||
|
0x2F85–0x2FA7 |
12166–12200 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |