Counter Commands
Preset Counters
The user can read the values of the counters from registers 571 to 578.
To preset the counters, the user must set up the command registers as follows:
| Address | Register | X | Unit | Type | Range | Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
42638 |
Command code = 42638 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
22 |
Number of parameters (bytes) = 22 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4353 |
Destination = 4353 (0x1100) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
1 |
– |
INT16U |
0–65535 |
0–65534 = preset value of the OF counter 65535 = do not preset the OF counter |
|
0x1F46 |
8007 |
1 |
– |
INT16U |
0–65535 |
0–65534 = preset value of the SD counter 65535 = do not preset the SD counter |
|
0x1F47 |
8008 |
1 |
– |
INT16U |
0–65535 |
0–65534 = preset value of the SDE counter 65535 = do not preset the SDE counter |
|
0x1F48 |
8009 |
1 |
– |
INT16U |
0–65535 |
0–65534 = preset value of the open circuit breaker command counter 65535 = do not preset the open circuit breaker command counter |
|
0x1F49 |
8010 |
1 |
– |
INT16U |
0–65535 |
0–65534 = preset value of the close circuit breaker command counter 65535 = do not preset the close circuit breaker command counter |
|
0x1F4A |
8011 |
1 |
– |
INT16U |
0–65535 |
0–65534 = preset value of the reset circuit breaker command counter 65535 = do not preset the reset circuit breaker command counter |
Set Up Thresholds
The user can read the values of the thresholds from registers 581 to 582.
To set up the thresholds, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
42639 |
Command code = 42639 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
22 |
Number of parameters (bytes) = 22 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4353 |
Destination = 4353 (0x1100) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
1 |
– |
INT16U |
0–65535 |
0–65534 = value of the OF counter threshold 65535 = do not change the OF counter threshold |
|
0x1F46 |
8007 |
1 |
– |
INT16U |
65535 |
65535 (no threshold is set up for the SD counter) |
|
0x1F47 |
8008 |
1 |
– |
INT16U |
65535 |
65535 (no threshold is set up for the SDE counter) |
|
0x1F48 |
8009 |
1 |
– |
INT16U |
65535 |
65535 (no threshold is set up for the open circuit breaker command counter) |
|
0x1F49 |
8010 |
1 |
– |
INT16U |
0–65535 |
0–65534 = value of the close circuit breaker command counter threshold 65535 = do not change close circuit breaker command counter threshold |
|
0x1F4A |
8011 |
1 |
– |
INT16U |
65535 |
65535 (no threshold is set up for the reset circuit breaker command counter) |