Event History
General Description
The BSCM Modbus SL/ULP module event history registers describe the last 10 events. The BSCM Modbus SL/ULP module event format corresponds to a series of 10 records. Each record is composed of 5 registers describing one BSCM Modbus SL/ULP module event.
A read request of 5x(n) registers is necessary to read the last n BSCM Modbus SL/ULP module event records, where 5 is the number of registers for each event record.
For example, a read request of 5x3 = 15 registers is necessary to read the last 3 BSCM Modbus SL/ULP module event records of the BSCM Modbus SL/ULP module event history:
-
The first 5 registers describe the first BSCM Modbus SL/ULP module event record (most recent event).
-
The next 5 registers describe the second BSCM Modbus SL/ULP module event record.
-
The last 5 registers describe the third BSCM Modbus SL/ULP module event record.
|
Address |
Register |
Description |
|---|---|---|
|
0x0259 |
602 |
Event counter |
|
0x025A–0x025E |
603–607 |
Event record 1 (most recent event) |
|
0x025F–0x0263 |
608–612 |
Event record 2 |
|
0x0264–0x0268 |
613–617 |
Event record 3 |
|
0x0269–0x026D |
618–622 |
Event record 4 |
|
0x026E–0x0272 |
623–627 |
Event record 5 |
|
0x0273–0x0277 |
628–632 |
Event record 6 |
|
0x0278–0x027C |
633–637 |
Event record 7 |
|
0x027D–0x0281 |
638–642 |
Event record 8 |
|
0x0282–0x0286 |
643–647 |
Event record 9 |
|
0x0287–0x028B |
648–652 |
Event record 10 (oldest event) |
Event Counter
The event counter is incremented when a new event is logged. If the counter reaches the maximum value 65535 and a new event is logged, the counter is reset to 0.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x0259 |
602 |
R |
1 |
– |
INT16U |
0–65535 |
BSCM Modbus SL/ULP module event counter |
Event Record
The order and the description of the event record registers are the same as that of event record 1:
|
Event 1 (Most Recent Event) |
|||||||
|---|---|---|---|---|---|---|---|
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|
0x025A |
603 |
R |
1 |
– |
INT16U |
0–65535 |
BSCM Modbus SL/ULP module event identifier (see next paragraph) |
|
0x025B–0x025D |
604–606 |
R |
– |
– |
ULP DATE |
– |
Date and time of event Data Type: ULP DATE |
|
0x025E |
607 |
R |
1 |
– |
INT16U |
1–2 |
Event status 1 = event occurrence 2 = event completion |
Event Identifier
|
Event Identifier |
Event |
|---|---|
|
1024 |
SD contact change (occurrence = close to SD position) |
|
1025 |
Threshold of OF counter is reached |
|
1026 |
Threshold of close command counter is reached |
|
1027 |
STOP (internal failure) |
|
1028 |
ERROR (internal failure) |
|
1029 |
OF contact change (occurrence = open to close position) |
|
1030 |
SDE contact change (occurrence = close to SDE position) |
|
1031 |
Manu/auto mode (occurrence = manu to auto position) |
|
1040 |
Open command |
|
1041 |
Close command |
|
1042 |
Reset command |