Schematics With ComPacT NSX Circuit Breakers
General Description
Depending on the type of circuit breaker used, the user must connect the IFM communication interface using one of the following configurations:
-
Connection of the IFM communication interface to the MicroLogic 5, 6 or 7 trip unit.
-
Connection of the IFM communication interface to the BSCM Modbus SL/ULP module.
-
Connection of the IFM communication interface to the BSCM Modbus SL/ULP module and the MicroLogic 5, 6 or 7 trip unit.
For more information, refer to DOCA0093•• ULP System User Guide.
ULP Connection
All connection configurations require the NSX cord or the insulated NSX cord.
DANGER |
|---|
|
hazard of electric shock, explosion or arc flash
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
Connection of the IFM Communication Interface to the MicroLogic 5, 6 or 7 Trip Unit
Connection of the IFM Communication Interface to the BSCM Modbus SL/ULP Module
Connection of the IFM Communication Interface to the BSCM Modbus SL/ULP Module and to the MicroLogic 5, 6 or 7 Trip Unit
Connection of the IFM Communication Interface to a Circuit Breaker for System Voltage Greater Than 480 Vac or 480 Vdc
DANGER |
|---|
|
hazard of electric shock, explosion or arc flash
Failure to follow these instructions will result in death or serious injury.
|
DANGER