IO Module Identification
Introduction
The order and the description of the IO module identification registers for IO 2 are the same as those of IO 1.
Addresses and Registers List
The following table describes the identification addresses, and registers regarding the IO module.
|
IO Module |
Addresses |
Registers |
|---|---|---|
|
IO 1 |
0x392F–0x3982 |
14640–14723 |
|
IO 2 |
0x44E7–0x453A |
17640–17723 |
IMU Identification
Identification of the IMU can be set by using EcoStruxure Power Commission software. When not programmed, the IMU identification registers return 0 (0x0000).
The FDM121 displays the first 14 characters of the IMU name.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3931–0x3948 |
14642–14665 |
R |
– |
OCTET STRING |
– |
IMU name = up to 45 ASCII characters ended by the NULL character 0x00 |
|
0x3949–0x3960 |
14666–14689 |
R |
– |
OCTET STRING |
– |
IMU location = up to 45 ASCII characters ended by the NULL character 0x00 |
IO Hardware Revision
The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:
-
XXX = major version (000–127)
-
YYY = minor version (000–255)
-
ZZZ = revision number (000–255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3961–0x3966 |
14690–14695 |
R |
– |
OCTET STRING |
– |
Hardware revision |
IO Module Firmware Revision
The firmware revision is an ASCII string using the format XXX.YYY.ZZZ with:
-
XXX = major version (000–127)
-
YYY = minor version (000–255)
-
ZZZ = revision number (000–255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3967–0x396C |
14696–14701 |
R |
– |
OCTET STRING |
– |
Firmware revision |
Current Date and Time
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x396D–0x3970 |
14702–14705 |
R |
– |
DATETIME |
– |
Current date and time of the IO module in DATETIME format, set by using EcoStruxure Power Commission software. |
Serial Number
The IO module serial number is composed of a maximum of 11 alphanumeric characters with the following format: PPYYWWDnnnn.
-
PP = plant code
-
YY = year of fabrication (05–99)
-
WW = week of fabrication (01–53)
-
D = day of fabrication (1–7)
-
nnnn = production number of the device on the day (0001–9999)
A read request of 6 registers is necessary to read the IO module serial number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3971–0x397A |
14706-14715 |
R |
– |
OCTET STRING |
– |
Serial number |
|
0x3971 |
14706 |
R |
– |
OCTET STRING |
– |
‘PP’ |
|
0x3972 |
14707 |
R |
– |
OCTET STRING |
‘05’–‘99’ |
‘YY’ |
|
0x3973 |
14708 |
R |
– |
OCTET STRING |
‘01’–‘53’ |
‘WW’ |
|
0x3974 |
14709 |
R |
– |
OCTET STRING |
‘10’–‘79’ |
‘Dn’ |
|
0x3975 |
14710 |
R |
– |
OCTET STRING |
‘00’–‘99’ |
‘nn’ |
|
0x3976 |
14711 |
R |
– |
OCTET STRING |
‘0’–‘9’ |
‘n’ (the NULL character ends the serial number) |
Manufacturing Date and Time
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x397B–0x397E |
14716–14719 |
R |
– |
DATETIME |
– |
Manufacturing date and time |
Product Identification
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x392F |
14640 |
R |
– |
INT16U |
15150 |
Product identification = 15150 for the IO module |
|
0x3930 |
14641 |
– |
– |
– |
– |
Reserved |
|
0x397F–0x3982 |
14720–14723 |
R |
– |
OCTET STRING |
– |
Product code = ‘LV434063’ |
|
0x3D1C–0x3D3B |
15645–15676 |
R–WC |
– |
OCTET STRING |
– |
User application name |
|
0x3D3C–0x3D45 |
15677–15686 |
R |
– |
OCTET STRING |
– |
Vendor name = ‘Schneider Electric’ |
|
0x3D46–0x3D4D |
15687–15694 |
R |
– |
OCTET STRING |
– |
Product range: ‘Enerlinx’ |
|
0x3D4E–0x3D5D |
15695–15710 |
R |
– |
OCTET STRING |
– |
Device family: ‘IO device’ |
|
0x3D5E–0x3D65 |
15711–15718 |
R |
– |
OCTET STRING |
– |
Product model |