Time-Stamped Information
General Description
The time-stamped information enables the user to know all the dates relative to important information such as previous protection settings and minimum/maximum values of currents, voltages, and system frequency.
The time-stamped information table describes:
-
the previous protection setup parameters and corresponding dates
-
the minimum and maximum values of voltage measurements and corresponding dates
-
the maximum values of current measurements and corresponding dates
-
the minimum and maximum system frequencies and corresponding dates
-
the peak demand of current and power and corresponding dates
A read request of 100 registers is necessary to read the time-stamped previous protection registers (29600–29699).
Previous Long-Time Protection Setup
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x739F |
29600 |
R |
1 |
A |
INT16U |
– |
Previous Ir pick-up value. The Ir range depends on the nominal current In. |
|
0x73A0– 0x73A2 |
29601– 29603 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73A3 |
29604 |
R |
1 |
ms |
INT16U |
500– 16000 |
Previous tr time delay (distribution application) tr = 500, 1000, 2000, 4000, 8000, 16000 ms |
|
0x73A4– 0x73A6 |
29605– 29607 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73A7 |
29608 |
R |
1 |
– |
INT16U |
5–30 |
Motor class (motor application only) Possible values = 5, 10, 20, 30 s |
|
0x73A8– 0x73AA |
29609– 29611 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73AB |
29612 |
R |
– |
– |
INT16U |
1–2 |
Previous cool fan setup (motor application only) 1 = auto, 2 =motor |
|
0x73AC– 0x73AE |
29613– 29615 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
Previous Short-Time Protection Setup
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73AF |
29616 |
R |
10 |
– |
INT16U |
(1) |
Previous Isd coefficient pick-up value |
|
0x73B0– 0x73B2 |
29617– 29619 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73B3 |
29620 |
R |
1 |
ms |
INT16U |
0–400 |
Previous tsd time delay tsd = 0, 100, 200, 300, 400 ms If tsd = 0 ms, then I2t must be Off. |
|
0x73B4– 0x73B6 |
29621– 29623 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73B7 |
29624 |
R |
– |
– |
INT16U |
0–1 |
Previous type of protection: 0 = I2t On, 1 = I2t Off |
|
0x73B8– 0x73BA |
29625– 29627 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
(1) The Isd coefficient range depends on:
|
|||||||
Previous Instantaneous Protection Setup
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73BB |
29628 |
R |
10 |
– |
INT16U |
(1) |
Previous Ii coefficient pick-up value |
|
0x73BC– 0x73BE |
29629– 29631 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
(1) The Ii coefficient range depends on the circuit breaker size:
|
|||||||
Previous Ground-Fault Protection Setup
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73BF |
29632 |
R |
100 |
ms |
INT16U |
(1) |
Previous Ig coefficient pick-up value. |
|
0x73C0– 0x73C2 |
29633– 29635 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73C3 |
29636 |
R |
1 |
ms |
INT16U |
0–400 |
Previous tg time delay tg = 0, 100, 200, 300, 400 ms |
|
0x73C4– 0x73C6 |
29637– 29639 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73C7 |
29640 |
R |
– |
– |
INT16U |
0–1 |
Previous type of protection: 0 = I2t On, 1 = I2t Off |
|
0x73C8– 0x73CA |
29641– 29643 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
(1) The Ig coefficient range depends on the nominal current In and the MicroLogic trip unit rotary switch if it exists. For example, 0 (protection off) or 0.40 In to In in steps of 0.05. |
|||||||
Previous Earth-Leakage Protection Setup
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73CB |
29644 |
R |
1 |
mA |
INT16U |
– |
Previous IΔn |
|
0x73CC– 0x73CE |
29645– 29647 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73CF |
29648 |
R |
1 |
ms |
INT16U |
0–1000 |
Previous tΔn time delay tΔn = 0, 60, 150, 500, 1000 ms If IΔn = 0.03 mA, then TΔn = 0 ms. |
|
0x73D0– 0x73D2 |
29649– 29651 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
Previous Jam Protection Setup
The jam protection is available for motor application only.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73D3 |
29652 |
R |
– |
– |
INT16U |
0–2 |
Previous setup status: 0 = Off, 1 = On |
|
0x73D4– 0x73D6 |
29653– 29655 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73D7 |
29656 |
R |
10 |
– |
INT16U |
10–80 |
Previous Ijam coefficient pick-up value |
|
0x73D8– 0x73DA |
29657– 29659 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73DB |
29660 |
R |
1 |
s |
INT16U |
1–30 |
Previous tjam time delay |
|
0x73DC– 0x73DE |
29661– 29663 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
Previous Unbalance Protection Setup
The unbalance protection is available for motor application only.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73DF |
29664 |
R |
1 |
% |
INT16U |
10–40 |
Previous unbalance coefficient pick-up value |
|
0x73E0– 0x73E2 |
29665– 29667 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73E3 |
29668 |
R |
1 |
s |
INT16U |
1–10 |
Previous tunbal time delay |
|
0x73E4– 0x73E6 |
29669– 29671 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
Previous Underload Protection Setup
The underload protection is available for motor application only.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73E7 |
29672 |
R |
– |
– |
INT16U |
0–2 |
Previous setup status: 0 = Off, 1 = On |
|
0x73E8– 0x73EA |
29673– 29675 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73EB |
29676 |
R |
100 |
– |
INT16U |
30–90 |
Previous Iunderload coefficient pick-up value |
|
0x73EC– 0x73EE |
29677– 29679 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73EF |
29680 |
R |
1 |
s |
INT16U |
1–200 |
Previous tunderload time delay |
|
0x73F0– 0x73F2 |
29681– 29683 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
Previous Long-Start Protection Setup
The long-start protection is available for motor application only.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73F3 |
29684 |
R |
– |
– |
INT16U |
0–2 |
Previous setup status: 0 = Off, 1 = On |
|
0x73F4– 0x73F6 |
29685– 29687 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73F7 |
29688 |
R |
10 |
– |
INT16U |
10–50 |
Previous Ilongstart coefficient pick-up value |
|
0x73F8– 0x73FA |
29689– 29691 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
|
0x73FB |
29692 |
R |
1 |
s |
INT16U |
1–30 |
Previous tlongstart time delay |
|
0x73FC– 0x73FE |
29693– 29695 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
Previous Neutral Protection Setup
The neutral protection is only available when system type in register 3314 is 30 or 41 System Type.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x73FF |
29696 |
R |
– |
– |
INT16U |
0–3 |
Previous neutral coefficient pick-up value: 0 = Off 1 = 0.5 2 = 1.0 3 = OSN |
|
0x7400– 0x7402 |
29697– 29699 |
R |
– |
– |
ULP DATE |
– |
Date and time of the previous setup. |
Minimum/Maximum V12 Voltage Measurements
A read request of 48 registers is necessary to read the time-stamped minimum/maximum values of voltage, current, and frequency registers (29780–29827).
Register = 0 if voltage < 25 V.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x7453 |
29780 |
R |
1 |
V |
INT16U |
0–850 |
Minimum of RMS phase-to-phase voltage V12 |
|
0x7454– 0x7456 |
29781– 29783 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
|
0x7457 |
29784 |
R |
1 |
V |
INT16U |
0–850 |
Maximum of RMS phase-to-phase voltage V12 |
|
0x7458– 0x745A |
29785– 29787 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
Minimum/Maximum V23 Voltage Measurements
Register = 0 if voltage < 25 V.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x745B |
29788 |
R |
1 |
V |
INT16U |
0–850 |
Minimum of RMS phase-to-phase voltage V23 |
|
0x745C– 0x745E |
29789– 29791 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
|
0x745F |
29792 |
R |
1 |
V |
INT16U |
0–850 |
Maximum of RMS phase-to-phase voltage V23 |
|
0x7460– 0x7462 |
29793– 29795 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
Minimum/Maximum V31 Voltage Measurements
Register = 0 if voltage < 25 V.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x7463 |
29796 |
R |
1 |
V |
INT16U |
0–850 |
Minimum of RMS phase-to-phase voltage V31 |
|
0x7464– 0x7466 |
29797– 29799 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
|
0x7467 |
29800 |
R |
1 |
V |
INT16U |
0–850 |
Maximum of RMS phase-to-phase voltage V31 |
|
0x7468– 0x746A |
29801– 29803 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
Maximum I1 Current Measurement
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x746B |
29804 |
R |
1 |
A |
INT16U |
0–20xIn |
Maximum of RMS current on phase 1: I1 |
|
0x746C– 0x746E |
29805– 29807 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
Maximum I2 Current Measurement
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x746F |
29808 |
R |
1 |
A |
INT16U |
0–20xIn |
Maximum of RMS current on phase 2: I2 |
|
0x7470– 0x7472 |
29809– 29811 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
Maximum I3 Current Measurement
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x7473 |
29812 |
R |
1 |
A |
INT16U |
0–20xIn |
Maximum of RMS current on phase 3: I3 |
|
0x7474– 0x7476 |
29813– 29815 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
Maximum IN Current Measurement
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x7477 |
29816 |
R |
1 |
A |
INT16U |
0–20xIn |
Maximum of RMS current on neutral: IN |
|
0x7478– 0x747A |
29817– 29819 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
Minimum System Frequency
When the MicroLogic trip unit cannot calculate the frequency, it returns Not Evaluated = 32768 (0x8000).
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x747B |
29820 |
R |
10 |
Hz |
INT16U |
150–4400 |
Minimum of system frequency |
|
0x747C– 0x747E |
29821– 29823 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
Maximum System Frequency
When the MicroLogic trip unit cannot calculate the frequency, it returns Not Evaluated = 32768 (0x8000).
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x747F |
29824 |
R |
10 |
Hz |
INT16U |
150–4400 |
Maximum of system frequency |
|
0x7480– 0x7482 |
29825– 29827 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
I1 Peak Demand Measurement
A read request of 20 registers is necessary to read the time-stamped peak demand of current and power (29828–29847).
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x7483 |
29828 |
R |
1 |
A |
INT16U |
0–20xIn |
I1 peak demand |
|
0x7484– 0x7486 |
29829– 29831 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
I2 Peak Demand Measurement
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x7487 |
29832 |
R |
1 |
A |
INT16U |
0–20xIn |
I2 peak demand |
|
0x7488– 0x748A |
29833– 29835 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
I3 Peak Demand Measurement
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x748B |
29836 |
R |
1 |
A |
INT16U |
0–20xIn |
I3 peak demand |
|
0x748C– 0x748E |
29837– 29839 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
IN Peak Demand Measurement
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x748F |
29840 |
R |
1 |
A |
INT16U |
0–20xIn |
IN peak demand |
|
0x7490– 0x7492 |
29841– 29843 |
R |
– |
– |
ULP DATE |
– |
Date and time. |
P Peak Demand Measurement
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x7493 |
29844 |
R |
10 |
kW |
INT16 |
-30000– +30000 |
P peak demand |
|
0x7494– 0x7496 |
29845– 29847 |
R |
– |
– |
ULP DATE |
– |
Date and time. |