Configuration of the SDx Module
Output 1
A read request of 3 registers is necessary to read the output 1 parameters.
The user can check the status and the validity of output 1 at register 8857.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x2648 |
9801 |
R |
1 |
– |
INT16U |
0–4 |
Output mode 0 = normal mode 1 = latched mode 2 = time delayed mode 3 = closed forced mode 4 = open forced mode |
|
0x2649 |
9802 |
R |
1 |
s |
INT16U |
1–360 |
Delay (if the output mode is set to 2). The factory setting is 1 s. |
|
0x264A |
9803 |
R |
1 |
– |
INT16U |
0–65535 |
Alarm identifier (201–210, 1013, 1014, 1015). The alarm identifier is set to 0 if there is no alarm. |
Output 2
A read request of 3 registers is necessary to read the output 2 parameters.
The user can check the status and the validity of output 2 at register 8857.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x264F |
9808 |
R |
1 |
– |
INT16U |
0–4 |
Output mode 0 = normal mode 1 = latched mode 2 = time delayed mode 3 = closed forced mode 4 = open forced mode |
|
0x2650 |
9809 |
R |
1 |
s |
INT16U |
1–360 |
Delay (if the output mode is set to 2). The factory setting is 1 s. |
|
0x2651 |
9810 |
R |
1 |
– |
INT16U |
0–65535 |
Alarm identifier (201–210, 1013, 1014, 1015). The alarm identifier is set to 0 if there is no alarm. |