Demand Measurements
General Description
Demand registers include:
-
current demand
-
active, reactive, and apparent power demand
The window duration of current demand depends on the configuration of register 3352. Refer to Demand Time.
The window duration and the window type of power demand depend on the configuration of registers 3354 and 3355. Refer to Demand Time.
The demand measurements are refreshed every minute with the sliding window type.
The demand measurements are refreshed at the end of the window interval with the block window type.
Current Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x0897 |
2200 |
R |
1 |
A |
INT16U |
0–20xIn |
Current demand on phase 1: I1 Dmd |
|
0x0898 |
2201 |
R |
1 |
A |
INT16U |
0–20xIn |
Current demand on phase 2: I2 Dmd |
|
0x0899 |
2202 |
R |
1 |
A |
INT16U |
0–20xIn |
Current demand on phase 3: I3 Dmd |
|
0x089A |
2203 |
R |
1 |
A |
INT16U |
0–20xIn |
Current demand on the neutral: IN Dmd (1) |
|
0x089B |
2204 |
R |
1 |
A |
INT16U |
0–20xIn |
Maximum of current demand on phase 1: I1 Peak Dmd (2) |
|
0x089C |
2205 |
R |
1 |
A |
INT16U |
0–20xIn |
Maximum of current demand on phase 2: I2 Peak Dmd (2) |
|
0x089D |
2206 |
R |
1 |
A |
INT16U |
0–20xIn |
Maximum of current demand on phase 3: I3 Peak Dmd (2) |
|
0x089E |
2207 |
R |
1 |
A |
INT16U |
0–20xIn |
Maximum of current demand on the neutral: IN Peak Dmd (1) (2) |
|
(1) This value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. (2) This value can be reset with the reset minimum/maximum command. Refer to Reset Minimum/Maximum. |
|||||||
Active Power Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x08AF |
2224 |
R |
10 |
kW |
INT16 |
-30000–+30000 |
Total active power demand: P Dmd (1) |
|
0x08B0 |
2225 |
R |
10 |
kW |
INT16 |
-30000–+30000 |
Maximum of total active power demand: P Peak Dmd (2) |
|
(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every minute. (2) This value can be reset with the reset minimum/maximum command. Refer to Reset Minimum/Maximum. |
|||||||
Reactive Power Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x08B5 |
2230 |
R |
10 |
kVAR |
INT16 |
-30000–+30000 |
Total reactive power demand: Q Dmd (1) |
|
0x08B6 |
2231 |
R |
10 |
kVAR |
INT16 |
-30000–+30000 |
Maximum of total reactive power demand: Q Peak Dmd (2) |
|
(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every minute. (2) This value can be reset with the reset minimum/maximum command. Refer to Reset Minimum/Maximum. |
|||||||
Apparent Power Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x08BB |
2236 |
R |
10 |
kVA |
INT16 |
0–30000 |
Total apparent power demand: S Dmd (1) |
|
0x08BC |
2237 |
R |
10 |
kVA |
INT16 |
0–30000 |
Maximum of total apparent power demand: S Peak Dmd (2) |
|
(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every minute. (2) This value can be reset with the reset minimum/maximum command. Refer to Reset Minimum/Maximum. |
|||||||